S12ZVM Toolbox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVM Toolbox

2,091件の閲覧回数
ashwin_raju
Contributor I

Will S12ZVM toolbox work in Matlab 2018b 64 bit or only in 32 bit?

0 件の賞賛
返信
2 返答(返信)

1,995件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

MATLAB 2018b is only available on 64-bit. The last MATLAB version that had 32-bit was 2015b. If you're planning on running the S12ZVM Toolbox on a newer version (2016b - 2018b) you'll have to install hotfix #2 (available here). We recommend you install all available hotfixes (available on the same link mentioned before).

P.S.: Keep in mind that this is an older toolbox that was released with support for MATLAB versions R2013a - R2015b (both 32bit and 64bit). We're maintaining support for later versions on a best-effort basis, so even though we provide hotfixes to make it usable in later versions, we do not guarantee all the features work as expected. If you're having issues running on a newer version, please post it on the community.

Kind regards,

Razvan.

0 件の賞賛
返信

1,994件の閲覧回数
ashwin_raju
Contributor I

Hello Razvan,

Thank you very much for the information.

Kind Regards

Ashwin Raju

0 件の賞賛
返信