HotFix: MBD Toolbox rev1.2.0 for MC9S12ZVMx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HotFix: MBD Toolbox rev1.2.0 for MC9S12ZVMx

3,530 Views
Daniel_Popa
NXP Employee
NXP Employee

HotFix_1: Send multiple CAN messages

NXP Tracking number: AST-606

 

Problem: When trying to sent multiple can messages from S12ZVMx targets using different CAN IDs the application sends only one message:

 

Root Cause: Coding logic error

 

Workaround:  Update the files attached in the following folders 

{Toolbox install dir}\mctbx_9s12zvm\mctbx_s12zvm\src\c_library\ folder mscan0_s12zvm.c file

{Toolbox install dir}\mctbx_9s12zvm\mctbx_s12zvmc256\src\c_library\ forder mscan0_s12zvmc256.c file

 

Customer Report: How do I send more than one CAN message? 

Special thanks to eungsoo Lee for testing and fix confirmation

Original Attachment has been moved to: mscan0_s12zvmc256.c.zip

Original Attachment has been moved to: mscan0_s12zvm.c.zip

Labels (1)
2 Replies

2,663 Views
constantinrazva
NXP Employee
NXP Employee

HotFix_2: Fix "Undefined function 'slsfnagctlr'..." when trying to generate code on R2016b/R2017a

 

Problem: If you try to generate code for any model on R2016b/R2017a, you will receive this error: "Undefined function 'slsfnagctlr' for input arguments of type 'char'." 

 

Root Cause: Matlab API change.

 

Workaround:  Download slsfnagctlr.p in the following folder

{Toolbox install dir}\mbdtbx_s12zvc\mbdtbx_s12zvc\mscripts

0 Kudos
Reply

2,663 Views
basilmathew
Contributor III

 Undefined function    'slsfnagctlr'    for input arguments of type    'char'

The above fix helped me to generate my code for MINIBRD S12VML , not connected the hardware hope , will work :smileyhappy:

0 Kudos
Reply