MR-CANHUBK344 programming from MBDT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MR-CANHUBK344 programming from MBDT

1,235 次查看
Chibi
Contributor I

How can I program the MR-CANHUBK344 board using the S32 Debug probe with application generated using MBDT?

0 项奖励
回复
3 回复数

1,160 次查看
robertv
NXP Employee
NXP Employee

Hello Chibi,

Unfortunately, the S32 Debug Probe does not provide support for S32K3, so it cannot be used to program the MR-CANHUBK344.

robertv_0-1698664350753.png
Programming the MR-CANHUBK344 board can be done using a J-Link Mini. The process of setting up the board, creating a model with MBDT and downloading the program to the board (using the J-Link Mini) is described in this newly written article that focuses on the MR-CANHUBK344: https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Interacting-with-Digital-Inputs-Outputs-on...

Regards, 
Robert V 

0 项奖励
回复

1,149 次查看
Chibi
Contributor I

Thank you for the response. Is there a similar documentation available to configure CAN and SPI drivers?

0 项奖励
回复

1,142 次查看
robertv
NXP Employee
NXP Employee

Hello Chibi,

Currently, the article I mentioned is the only one in the series that has been published. Soon, more articles will be published covering more peripherals.
One of them is focused around CAN communication on the MR-CANHUBK344 and it should be available in a few weeks.

Regards, 
Robert V

0 项奖励
回复