Not able to configure the pins through S32 Configuration tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Not able to configure the pins through S32 Configuration tool

1,311 次查看
Dbhangale
Contributor I

I configured the pins in the S32 Configuration tool but I cannot see the pins available in the Simulink blocks. For Example I configured PTD28[134] as a digital Input pin but the Simulink DOI read channel block does not show the pin option. Also when I start the S32 configure tool I am getting error Shown below. SLF4J: Failed to load class "org.slf4j.impl.StaticLoggerBinder". SLF4J: Defaulting to no-operation (NOP) logger implementation SLF4J: See http://www.slf4j.org/codes.html#StaticLoggerBinder for further details.

0 项奖励
回复
1 回复

1,285 次查看
Irina_Costachescu
NXP Employee
NXP Employee

Hi @Dbhangale ,

For the pins configured inside the S32 Configuration Tools (Pins Tool) to be visible inside the DIO Simulink block provided by MBDT, the Dio channels corresponding to those pins must also be configured inside the Dio component. The following article (sections 2.2 and 2.3), available on our NXP Community, provides a step by step tutorial of how pins must be configured inside a .mex file and how they can be used inside a Simulink model.

Related to the second item, these messages are not related to an error, and they are coming from eclipse (platform over which S32 Configuration Tools is developed) and they should not impact the workflow MBDT proposes for configuring the target using S32 Configuration Tools. You should be able to open the configuration and modify it as required for your application particularities.

Please let us know in case you encounter any issues while using MBDT.

Thank you,

Irina

0 项奖励
回复