How to export Generated Code to S32 Design Studio IDE (applicable for MBDT for MPC5744P v2.0)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to export Generated Code to S32 Design Studio IDE (applicable for MBDT for MPC5744P v2.0)

62,427件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

In case you need to export the generated code to S32 Design Studio for PA IDE, now there is an easy way. No more painful job of reconstruction the project manually and setting all sort of compiler flags. Here is what you need to do in just a few steps.

Prerequisite:

Toolbox for MPC5744P rev2.0: Model Based Design Toolbox For Panther (MPC574xP) Family of Processors 2.0 IS NOW AVAILABLE! 

HotFix_4 for MPC5744P rev2.0: https://community.nxp.com/thread/451804#comment-925214 

S32DS IDE v1.2 or newer:  S32 Design Studio for Power v1.2.

How to:

#1: make sure the HotFix_4 is installed successfully and the "Generated S32 Design Studio ProjectInfo.xml file" option is visible and selected

pastedImage_5.png

#2: build the Simulink model as normal (e.g. Motor Control System example from Motor Control Class: Lecture 12 - Motor Control System since it is the most complex application we built so far on this community) and wait until is completed successfully.

pastedImage_123.png

 

#3: Open S32DS for PA and select Import/S32 Design Studio/ProjectInfo.xml Importer

pastedImage_124.png

#4: Press Next and select the ProjectInfo.xml from the location used to generated the C-code for the Simulink model. Also, select the E200 Executable option

pastedImage_166.png

#5: Click on Finish button to have the project imported into the S32 Design Studio workspace.

pastedImage_168.png

#6: Applicable for S32DS v1.2 (due to a bug in IDE): Open the Project Properties and go to Settings/Target Processor and select "generate code for E200Z4" as Target Processor and re=select the option shown near the Libraries Support. These will force the IDE to update the toolchain properties correctly. These limitations will be addressed in the newer versions of S32DS for PA.  

pastedImage_169.png

#7: Build the project

pastedImage_175.png

Expected result: The executable file should be produced without any errors. In case of errors - please recheck #6.

pastedImage_178.png

52 返答(返信)

26,636件の閲覧回数
orson_CZCN
Contributor I

There is no target compiler opts in my code generation configuration

orson_CZCN_0-1723186978415.pngorson_CZCN_0-1723186978415.png

Where exactly can I set up to open the generated project in the S32K DS!!!

0 件の賞賛
返信

37,106件の閲覧回数
hbhnhbnhj1
Contributor III

Hi @Daniel_Popa @mariuslucianand 

After I follow the instruction above, the build process cannot success.

The building environment is as follow, 

*OS : Windows 11 21H2

hbhnhbnhj1_1-1649662387169.pnghbhnhbnhj1_1-1649662387169.png

*Matlab : R2018a with MBD Toolbox v3.2

hbhnhbnhj1_3-1649662410853.pnghbhnhbnhj1_3-1649662410853.png

hbhnhbnhj1_2-1649662405569.pnghbhnhbnhj1_2-1649662405569.png

*S32DS : v2.1

hbhnhbnhj1_0-1649662368371.pnghbhnhbnhj1_0-1649662368371.png

*MPC5744P : rev B


The Simulink model I build to test is【uart_hello_world_mpc574xP.mdl】from MBD Toolbox v3.2, I attached the file as【uart_hello_world_mpc574xP.zip】.
hbhnhbnhj1_5-1649662566104.pnghbhnhbnhj1_5-1649662566104.png

The build process of model is shown as attached file 【uart_hello_world_mpc574xP_matlab_build_20220411.txt】, in short, it build completely as figure below.

hbhnhbnhj1_7-1649662698384.pnghbhnhbnhj1_7-1649662698384.png
The generated file is attached as【uart_hello_world_mpc574xP_mbd_rtw.zip】.


Then I load the xml of this project to S32DS for building, the result is as figure below, 

hbhnhbnhj1_8-1649662874402.pnghbhnhbnhj1_8-1649662874402.png

However, the building result is failed because of the issue as figure below, 

hbhnhbnhj1_10-1649662976303.pnghbhnhbnhj1_10-1649662976303.png
log of detailed building is shown in attached file【uart_hello_world_mpc574xP_s32_build_20220411.txt】.

By the way, if I build model with CAN, it will show that 【can_message.h】is missing, I found it at Matlab installation directory.
I copy it to the directory where the project is build ( should it be automatically access with xml of project ? ),
the error is eliminated but it still cannot be successfully build for the same reason as【uart_hello_world_mpc574xP】.

Please give me guidance, thank you!!

タグ(4)
0 件の賞賛
返信

36,844件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @p_a_u_darshana,

As @hbhnhbnhj1 mentioned in a comment, you have to rename the extension of those 3 files from the capital ".S" into lower ".s". You shall do that inside the ProjectInfo.xml also, just before importing it into S32DS.

As for the can_message.h, you have to add that file manually after importing the ProjectInfo.xml into S32DS, as you already mention that this process solves this error. In my generated code for some CAN examples, I was not able to find this file. Are you using some custom code or external can files?

Hope this helps,

Marius

 

 

タグ(1)
0 件の賞賛
返信

35,387件の閲覧回数
p_a_u_darshana
Contributor III

Hello @mariuslucianand 

 

Sorry for the late reply. 

We have to have this "can_message.h" file when we use CAN pack/ CAN unpack blocks in our model. In your case, NXP examples do not use this block to Pack/Unpack individual signals into/from CAN messages.

We have to go to the Matlab folder in C drive to find this  "can_message.h". It is coming with 

In my case I have found this  "can_message.h" file in the "MATLAB\R2021b\toolbox\shared\can\src\scanutil" folder

thank you

0 件の賞賛
返信

37,056件の閲覧回数
hbhnhbnhj1
Contributor III

Hi @dumitru-daniel_ @mariuslucianand,

This issue was raised before, it was solved as follow, sorry to bother you.
Re: How to export Generated Code to S32 Design Stu... - NXP Community

0 件の賞賛
返信

36,890件の閲覧回数
p_a_u_darshana
Contributor III

@hbhnhbnhj1 

Hi,

So did you just use the older version of DS IDE to solve this?

 

thank you.

0 件の賞賛
返信

36,887件の閲覧回数
hbhnhbnhj1
Contributor III

hi @p_a_u_darshana ,

I modifed the filename extension from .S to .s, then the error is cleared.

36,880件の閲覧回数
p_a_u_darshana
Contributor III

Hi @hbhnhbnhj1

How about the [can_message.h]? I also have the same error. I could not find this file. 

Can you give me more details about the way you solve this error?

Thank you

 

 

0 件の賞賛
返信

38,631件の閲覧回数
p_a_u_darshana
Contributor III

Hi @mariuslucianand @Daniel_Popa 

I followed all the steps as mentioned in this post but I cannot build the project.

After I export the generated code to the S32DS the build option is disabled automatically.

p_a_u_darshana_0-1636526868050.pngp_a_u_darshana_0-1636526868050.png

 

Maybe this is due to the spaces in the MBD toolbox path.

C:\Users\user\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx(3)

Can you please let me know how to change the installation path? There are no options to select the installation path when we install the toolbox.

Thank you.

0 件の賞賛
返信

38,599件の閲覧回数
gwwang
Contributor I

You can change the default installation path by changing the path in MATLAB - Preferences - MATLAB - Add-Ons.

タグ(2)

40,140件の閲覧回数
vietmai
Contributor I

Hi @Daniel_Popa @constantinrazva 

My S32 is not able to build after importing xml project file generated by Simulink.

vietmai_0-1613701266071.pngvietmai_0-1613701266071.png 

vietmai_0-1613701412673.pngvietmai_0-1613701412673.png

 

Below are details what i did, 

i checked the installation path of NXP MBD, whether it has "space" in the directory of not : 

C:\Users\vietmq\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32K1xx         ==> Should be OK, no space.

Open MBD GPIO example for S32K144, and configure for exporting xml project file: 

vietmai_1-1613702006437.pngvietmai_1-1613702006437.png

Generate the code, no error, see log file : gpio_s32k144_build_20210219_103350.txt (attached in the post)

Open S32SD and import xml file : 

vietmai_2-1613702311093.pngvietmai_2-1613702311093.png

i ticked on the first option, can not build, then i tried second option but can not build too. 

Please help !!!

 

thanks.

0 件の賞賛
返信

39,139件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @vietmai ,

Can you please attach the output of the S32DS when trying to build?

I have tried your model and on my machine, I was able to build it.

mariuslucianand_0-1630923490624.pngmariuslucianand_0-1630923490624.png

Regards,

Marius

0 件の賞賛
返信

40,849件の閲覧回数
lijiantaowy
Contributor III

Hello daniel

When I export Generated Code( MBDT for MPC5744P v3.2) to S32 Design Studio for Power Architecture Version 2017.R1, I can't build the project! The details are as follows.

pastedImage_6.png>pastedImage_7.png>pastedImage_9.png>pastedImage_10.png>pastedImage_11.png>build>pastedImage_12.pngpastedImage_13.png>importpastedImage_14.png>pastedImage_15.png>pastedImage_16.pngpastedImage_17.png

pastedImage_19.png

0 件の賞賛
返信

40,849件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected],

S32Design Studio has some hick-ups when it comes to paths with spaces -- and when you are trying to import the project generated by our toolbox, you'll be generating ProjectInfo.xml file which is then used as input for S32Design Studio importer. This XML file will contain a path to your toolbox, so it will contain spaces, and S32DS crashes somewhere. 

To fix this, you should install your toolbox in a path with no spaces - this is a general recommendation for everything (I guess).

Please let us know if you have any issues with it after installing it into a new path with no spaces.

Kind regards,

Razvan.

40,849件の閲覧回数
lijiantaowy
Contributor III

Hello!

Thank you, reinstall the toolbox in the path without spaces according to your promptthe problem is solved,. It turns out that there is a matlab add-on in the default path with spaces. However, the 3.0 version I installed before, there is no problem to install in that path.

Also I would like to ask, after installing version 3.2, compiling programs in matlab becomes very slow, the same program is significantly faster in version 3.0, can I change the settings to speed up compilation?

pastedImage_5.png

There is another problem. When I use the motor program in the toolbox, I need to add two paths each time I import it into S32. Is there any setting that can permanently solve this problem?

use thispastedImage_11.png> need to add paths>pastedImage_8.pngpastedImage_9.png>build successful

Best regards,

Jiantao

 

0 件の賞賛
返信

40,849件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected],

I'm glad everything worked out with the importer -- as for the default toolbox path, it depends on what MATLAB/Simulink version you are running - they will be slightly different (+ some will generate an extra folder named code, others will not).

Now for the compile time -- did you test the 2 versions of the toolbox on the same Simulink version? If you did, could you send us the model that you are running? It goes without saying that the build depends on the complexity of the model itself -- so it would be best if we could run some tests on the model you have here (the one which takes you 3m+ to build).

Kind regards,

Razvan.

0 件の賞賛
返信

40,849件の閲覧回数
lijiantaowy
Contributor III

Hello!

The test file is below

Best regards,

Jiantao

0 件の賞賛
返信

40,849件の閲覧回数
lijiantaowy
Contributor III

Hello!

MBD3.2 pastedImage_2.png

MBD3.0pastedImage_1.png

Detailed test information

NotebookCPU i7-9750H RAM 16G

Best regards

Jiantao

0 件の賞賛
返信

40,850件の閲覧回数
haoxue1027
Contributor V

Hi 

I try to build the project, but there is three errors like following,

I used the latest version of MBD and S32.

pastedImage_1.pngpastedImage_2.png

I also try to delete the following including paths 

 pastedImage_4.png

but still have errors 

pastedImage_5.png

pastedImage_6.png

the  defualt optio" for E20072"of  target processor   is the same errors.

May I have your help.

best regards

hao

0 件の賞賛
返信

40,850件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected],

Unfortunately that is an issue with S32 Design Studio (latest version). It will be fixed in the next update I think.

You can try a workaround for the moment, or with the S32 Design Studio version 2017.R1 (older version).

For the workaround, you should rename all .S files to .s files (so they don't use capital letter S)

e.g.:

core0_intc_sw_handlers.S - to core0_intc_sw_handlers.s
interrupt_vectors.S - to interrupt_vectors.s
startup_MPC5744P.S - to startup_MPC5744P.s

If this alone does not work, you should also rename the files in ProjectInfo.xml (generated by our toolbox).

If you try the workaround please let us know if you are facing issues.

If you just try the older version (2017.R1), it should work without any errors.

Kind regards,

Razvan.

0 件の賞賛
返信