Model-Based Design Toolbox For Panther (MPC574xP) Family of Processors 2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Model-Based Design Toolbox For Panther (MPC574xP) Family of Processors 2.0

Model-Based Design Toolbox For Panther (MPC574xP) Family of Processors 2.0

MODEL BASED DESIGN TOOLBOX FOR PANTHER (MPC574xP) Family of Processors 2.0

 

Model Based Design Toolbox for MATLAB/Simulink supporting Panther (MPC57xP) version 2.0 is now available.

 

The product is FREE OF CHARGE and it is available for public.

 

DOWNLOAD

Model Based Design Toolbox

MBDT

  

 

Release Highlights – Model Based Design Toolbox for Panther (MPC574xP)

  • Support for new Panther XDEVKIT-MPC5744P board (ARDUINO style) which works with the new chassis XDEVKIT-MOTORGD for motor control applications.
  • Incorporation of latest Automotive Math and Motor Control Library release 1.1.7.
  • Support for latest MATLAB versions including 64 bits (2015/2016 a/b)
  • New DMA blocks, allowing ADC sampled data to be transferred to memory without CPU intervention through DMA module.
  • New LINFlexD blocks for serial communication support now allowing data send/receive operations through UART.
  • New Memory Read/Write blocks are added and they can now be used to read/write any memory zone.
  • New Custom Initialization block is added and it can be used to extend the configuration of any module outside the default setup prior to the model first step.
  • Support for S32 Design Studio for Power Compiler v1.1 in addition to new compilers versions Wind River DIAB v5.9.4.8 and Green Hills MULTI for PowerPC v2015.1
  • New Advanced Motor Control blocks, were added and now new functions like Track Observer or Back EMF Observer are provided as Simulink Blocks.
  • Aligned ADC clock frequency from 20MHz to 80MHz (max speed).
  • New ADC channel configuration block is redesigned to be allow configuration without sampling for the ADC channel, making now DMA scenario for transfers possible.
  • New Diagnostics panel can be used to enable/disable multiple consistency checks.
  • New Bootloader build to support UART1 communication.
  • Support in sync with FreeMASTER release 2.0.2.

 

new!!! HOT-FIX:  Add support for the latest e200 compiler that is released with S32 Design Studio for Power v1.2 .

Refer to HotFix_3 setup to have the MBD Toolbox working with latest e200 compiler.

 

Community Support Available

 

Support available via the NXP community at: https://community.nxp.com/community/mbdt

Attachments
Comments

Hi Daniel,

I download the Toolbox,but i can not get the license.lic,

pastedImage_1.png

where can i get it?

Hi edenli, 

What you have downloaded is the Math and Motor Control Library that is separately from the Model-Based Design Toolbox.

For the library itself you do not need a license.

Best regards,

Daniel

Toolbox download link doesn't work

Hi chandan24,

It was probably just a glitch. In case it still not working for you, please use this direct link: https://nxp.flexnetoperations.com/control/frse/product?child_plneID=683951&cert_num=284425987 

or 

Use the Model-Based Design official page to get access to download locations: Model-Based Design Toolbox|NXP 

Hope this helps!
Daniel

No ratings
Version history
Last update:
‎02-20-2017 03:00 AM
Updated by: