How to Debug in MATLAB Without OpenSDA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to Debug in MATLAB Without OpenSDA

跳至解决方案
2,519 次查看
yyang
Contributor II

Dear engineer:

I do not have a demo board ,which integrated with OpenSDA .

I konw how to debug the *.elf file in S32DS, but I want to know can I use PE MULTILINK UNIVERSAL or Jlink to download the program to my target MCU(S32K or MPC7544P) in MATLAB ?

标记 (1)
0 项奖励
回复
1 解答
2,258 次查看
mariuslucianand
NXP Employee
NXP Employee

Hi yyang‌,

We are currently not supporting the programming of the controller using PE MULTILINK UNIVERSAL or J Link directly from Matlab. You can flash it either using the S32DS or from Matlab or you can try downloading it using the Serial port for that you need to  flash the bootloader(from {MBDT path}/mbdtbx_S32K\tools\BootLoader\RBF_Files) before.

Marius

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,259 次查看
mariuslucianand
NXP Employee
NXP Employee

Hi yyang‌,

We are currently not supporting the programming of the controller using PE MULTILINK UNIVERSAL or J Link directly from Matlab. You can flash it either using the S32DS or from Matlab or you can try downloading it using the Serial port for that you need to  flash the bootloader(from {MBDT path}/mbdtbx_S32K\tools\BootLoader\RBF_Files) before.

Marius

0 项奖励
回复