How to Debug in MATLAB Without OpenSDA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Debug in MATLAB Without OpenSDA

Jump to solution
2,585 Views
yyang
Contributor II

Dear engineer:

I do not have a demo board ,which integrated with OpenSDA .

I konw how to debug the *.elf file in S32DS, but I want to know can I use PE MULTILINK UNIVERSAL or Jlink to download the program to my target MCU(S32K or MPC7544P) in MATLAB ?

Tags (1)
0 Kudos
Reply
1 Solution
2,324 Views
mariuslucianand
NXP Employee
NXP Employee

Hi yyang‌,

We are currently not supporting the programming of the controller using PE MULTILINK UNIVERSAL or J Link directly from Matlab. You can flash it either using the S32DS or from Matlab or you can try downloading it using the Serial port for that you need to  flash the bootloader(from {MBDT path}/mbdtbx_S32K\tools\BootLoader\RBF_Files) before.

Marius

View solution in original post

0 Kudos
Reply
1 Reply
2,324 Views
mariuslucianand
NXP Employee
NXP Employee

Hi yyang‌,

We are currently not supporting the programming of the controller using PE MULTILINK UNIVERSAL or J Link directly from Matlab. You can flash it either using the S32DS or from Matlab or you can try downloading it using the Serial port for that you need to  flash the bootloader(from {MBDT path}/mbdtbx_S32K\tools\BootLoader\RBF_Files) before.

Marius

0 Kudos
Reply