How to Debug in MATLAB Without OpenSDA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Debug in MATLAB Without OpenSDA

ソリューションへジャンプ
2,480件の閲覧回数
yyang
Contributor II

Dear engineer:

I do not have a demo board ,which integrated with OpenSDA .

I konw how to debug the *.elf file in S32DS, but I want to know can I use PE MULTILINK UNIVERSAL or Jlink to download the program to my target MCU(S32K or MPC7544P) in MATLAB ?

タグ(1)
0 件の賞賛
返信
1 解決策
2,219件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hi yyang‌,

We are currently not supporting the programming of the controller using PE MULTILINK UNIVERSAL or J Link directly from Matlab. You can flash it either using the S32DS or from Matlab or you can try downloading it using the Serial port for that you need to  flash the bootloader(from {MBDT path}/mbdtbx_S32K\tools\BootLoader\RBF_Files) before.

Marius

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,220件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hi yyang‌,

We are currently not supporting the programming of the controller using PE MULTILINK UNIVERSAL or J Link directly from Matlab. You can flash it either using the S32DS or from Matlab or you can try downloading it using the Serial port for that you need to  flash the bootloader(from {MBDT path}/mbdtbx_S32K\tools\BootLoader\RBF_Files) before.

Marius

0 件の賞賛
返信