Free Master with MBDT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Free Master with MBDT

1,399件の閲覧回数
avinashstarkenn
Contributor III

Hello,

I am using MBDT for s32k3xx.

Please can you help with tutorial/documents for how to use freemaster with MBDT.

I am using free master to view adc value.Can you guide how to build model and then how to view value on FreeMaster.

0 件の賞賛
返信
1 返信

1,349件の閲覧回数
georgevictor
NXP Employee
NXP Employee

Hi, @avinashstarkenn,

 

First of all, I need to mention that the FreeMaster tool can be used through multiple connection types. I suggest you to use one of the following two based on your available hardware:

  1. Using a debug probe, and access the target microcontroller memory over BDM communication.

You can find a topic related to this type of connection at the following link on our community:

https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/FreeMaster-Documentation-How-to-Use-Fre...

  1. Using a serial communication.

In order to establish communication between the evaluation board and the FreeMaster tool, you must use a USB2Serial converter. The software and hardware configurations that need to be verified before using serial communication are covered in the following topic:

https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32K3X4EVB-Q257-with-MBDT/m-p/1703621#M...

FreeMaster, ExternalMode, or PiL can all use the serial communication configuration.

  1. Regarding the question on how to use FreeMaster, you can take a look at the following video, which presents a simple application that uses the FreeMaster tool together with the S32K1xx toolbox. The S32K1 workflow is a little bit different from the S32K3 one that you are using, but you can focus only on the last part, which is about the FreeMaster configuration:

https://community.nxp.com/t5/video/gallerypage/video-id/6185806973001

 The main idea here is to successfully generate an executable .elf file and then use it in FreeMaster to read the desired variable values.

 

Hope this helps.

Have a nice day,

Victor

0 件の賞賛
返信