What is the Time delay function in MQX? Using board Kwikstik K40

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the Time delay function in MQX? Using board Kwikstik K40

Jump to solution
2,448 Views
yasararafath
Contributor II

Hi all,

     I have just started working on MQX RTOS. In that i am not able to understand it.

     I need sample code and how to run the MQX application in KwikStik K40.

     And also i need a timer and delay function in that timer. If anybody can please...

0 Kudos
Reply
1 Solution
1,242 Views
c0170
Senior Contributor III

Hello,

What have you done so far?

Please review the code which is provided within MQX installation. There are examples for the Kwikstik. Firstly, build BSP and PSP for the Kwikstick board then run timer example.

More information available Chapter 3.8 TIMING in MQX User Guide.

Regards,

c0170

View solution in original post

0 Kudos
Reply
2 Replies
1,243 Views
c0170
Senior Contributor III

Hello,

What have you done so far?

Please review the code which is provided within MQX installation. There are examples for the Kwikstik. Firstly, build BSP and PSP for the Kwikstick board then run timer example.

More information available Chapter 3.8 TIMING in MQX User Guide.

Regards,

c0170

0 Kudos
Reply
1,242 Views
yasararafath
Contributor II

Thank You, Kojtal.

0 Kudos
Reply