What is the Time delay function in MQX? Using board Kwikstik K40

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the Time delay function in MQX? Using board Kwikstik K40

ソリューションへジャンプ
3,027件の閲覧回数
yasararafath
Contributor II

Hi all,

     I have just started working on MQX RTOS. In that i am not able to understand it.

     I need sample code and how to run the MQX application in KwikStik K40.

     And also i need a timer and delay function in that timer. If anybody can please...

タグ(5)
0 件の賞賛
返信
1 解決策
1,821件の閲覧回数
c0170
Senior Contributor III

Hello,

What have you done so far?

Please review the code which is provided within MQX installation. There are examples for the Kwikstik. Firstly, build BSP and PSP for the Kwikstick board then run timer example.

More information available Chapter 3.8 TIMING in MQX User Guide.

Regards,

c0170

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,822件の閲覧回数
c0170
Senior Contributor III

Hello,

What have you done so far?

Please review the code which is provided within MQX installation. There are examples for the Kwikstik. Firstly, build BSP and PSP for the Kwikstick board then run timer example.

More information available Chapter 3.8 TIMING in MQX User Guide.

Regards,

c0170

0 件の賞賛
返信
1,821件の閲覧回数
yasararafath
Contributor II

Thank You, Kojtal.

0 件の賞賛
返信