What is the Time delay function in MQX? Using board Kwikstik K40

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What is the Time delay function in MQX? Using board Kwikstik K40

跳至解决方案
3,025 次查看
yasararafath
Contributor II

Hi all,

     I have just started working on MQX RTOS. In that i am not able to understand it.

     I need sample code and how to run the MQX application in KwikStik K40.

     And also i need a timer and delay function in that timer. If anybody can please...

标记 (5)
0 项奖励
回复
1 解答
1,819 次查看
c0170
Senior Contributor III

Hello,

What have you done so far?

Please review the code which is provided within MQX installation. There are examples for the Kwikstik. Firstly, build BSP and PSP for the Kwikstick board then run timer example.

More information available Chapter 3.8 TIMING in MQX User Guide.

Regards,

c0170

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,820 次查看
c0170
Senior Contributor III

Hello,

What have you done so far?

Please review the code which is provided within MQX installation. There are examples for the Kwikstik. Firstly, build BSP and PSP for the Kwikstick board then run timer example.

More information available Chapter 3.8 TIMING in MQX User Guide.

Regards,

c0170

0 项奖励
回复
1,819 次查看
yasararafath
Contributor II

Thank You, Kojtal.

0 项奖励
回复