Intergrating projects in mqx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Intergrating projects in mqx

Jump to solution
3,443 Views
vibhu
Contributor III

Hi Guys,

I am using keil IDE and mqx 4.1. The board I am using is twr-k70f120m. I want to integrate two projects into a single project. 

1) Freescale_MQX_4_1\rtcs\examples\snmp

2) Freescale_MQX_4_1\mqx\examples\spi

3) Freescale_MQX_4_1\mfs\examples\sdcard

I want to integrate the above projects into a single project and the three project's functionality should work. How do I do it ? what files should I add and how do I add the libraries?

Please Help !

Regards,

Vibhu

0 Kudos
Reply
1 Solution
3,304 Views
danielchen
NXP TechSupport
NXP TechSupport

Yes, you also need to merge the include files for sdcard and spi into snmp project.

This same also applies to linker 

pastedImage_1.png

as you can see, snmp only linked bsp.lib and psp.lib,   since you will add sdcard,  then mfs.lib will be included here

Regards

Daniel

View solution in original post

0 Kudos
Reply
3 Replies
3,304 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Vibhu:

You can start with SNMP project, then add the other application code to the snmp project.

Libraies are the same.

You should also take care the user_config.h file, merge the 3 configuations into one file

Regards

Daniel

3,304 Views
vibhu
Contributor III

Hi Daniel,

Thank you for your reply !

Just for clarification, aren't the build files in separate folders like for sdcard it will be inside the mfs->source->include and for snmp it will be inside rtcs->source->include folder?

If I include #include <mfs.h> in snmp file it is giving header file not found.

Should I change anything in keil ?

Please Help.

Regards,

Vibhu

0 Kudos
Reply
3,305 Views
danielchen
NXP TechSupport
NXP TechSupport

Yes, you also need to merge the include files for sdcard and spi into snmp project.

This same also applies to linker 

pastedImage_1.png

as you can see, snmp only linked bsp.lib and psp.lib,   since you will add sdcard,  then mfs.lib will be included here

Regards

Daniel

0 Kudos
Reply