买了几个MK20DX128VFM5芯片,电路图见附件
将USB插入电脑,没有任何反应,识别不了USB口,
测试如下:
TP3003(VBAT): 0.659V
TP3002(EXTAL32):0V
TP3001(XTAL):0V
TP3012(ADC0):3.3V
GPIO20 GPIO19:0.017V
8MHz 晶振未起震
Hi,
VBAT provides power to 32KHz oscillator and RTC modules.
I would recommend customer to refer TWR-K20D50M board schematics about power and SWD debugger interface circuit.
The system oscillator and 32KHz oscillator need software to enable internally.
Please download and refer K20 50MHz bare-metal software here.
Wish it helps.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
First of all, sorry for the later reply.
I think you want to make MK20 works as on board OpenSDA debugger tool. Right?
If yes, I would recommend customer to check here for OpenSDA debugger tool resource.
The FRDM-K28F is using the latest OpenSDA v2.2 , which provided OpenSDA and bootloader firmware.
The OpenSDA circuit should refer FRDM-K28F board schematics .
Please let me know if there still with any updated query. Thanks.
Have a great day,
Mike
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi,hui_ma
If i want to make MK20 works as on board OpenSDA debugger tool on the DEVKITMPC5744P.
where to find OpenSDA debugger tool resource.
there is not an option for DEVKITMPC5744P.
best regards
hao
Hi Hao,
Could you post your question at MPC5xxx sub-forum?
My colleague could help with that thread. Thanks.
best regards,
Mike
hi Hui_Ma
thanks for your suggestion.
best regards,
hao