Intergrating projects in mqx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Intergrating projects in mqx

ソリューションへジャンプ
3,324件の閲覧回数
vibhu
Contributor III

Hi Guys,

I am using keil IDE and mqx 4.1. The board I am using is twr-k70f120m. I want to integrate two projects into a single project. 

1) Freescale_MQX_4_1\rtcs\examples\snmp

2) Freescale_MQX_4_1\mqx\examples\spi

3) Freescale_MQX_4_1\mfs\examples\sdcard

I want to integrate the above projects into a single project and the three project's functionality should work. How do I do it ? what files should I add and how do I add the libraries?

Please Help !

Regards,

Vibhu

0 件の賞賛
返信
1 解決策
3,185件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Yes, you also need to merge the include files for sdcard and spi into snmp project.

This same also applies to linker 

pastedImage_1.png

as you can see, snmp only linked bsp.lib and psp.lib,   since you will add sdcard,  then mfs.lib will be included here

Regards

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,185件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Vibhu:

You can start with SNMP project, then add the other application code to the snmp project.

Libraies are the same.

You should also take care the user_config.h file, merge the 3 configuations into one file

Regards

Daniel

3,185件の閲覧回数
vibhu
Contributor III

Hi Daniel,

Thank you for your reply !

Just for clarification, aren't the build files in separate folders like for sdcard it will be inside the mfs->source->include and for snmp it will be inside rtcs->source->include folder?

If I include #include <mfs.h> in snmp file it is giving header file not found.

Should I change anything in keil ?

Please Help.

Regards,

Vibhu

0 件の賞賛
返信
3,186件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Yes, you also need to merge the include files for sdcard and spi into snmp project.

This same also applies to linker 

pastedImage_1.png

as you can see, snmp only linked bsp.lib and psp.lib,   since you will add sdcard,  then mfs.lib will be included here

Regards

Daniel

0 件の賞賛
返信