Ethernet link status

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet link status

Jump to solution
1,679 Views
Tgomes
Contributor III

Hi everybody,

 

 

I'm trying to use the function "ipcfg_get_link_active" to figure out if an ethernet cable is connected or not, but it seems don't work as expected. The return is always true, even when the cable is unconnected. Is there any configuration that I can change or set for test and find the problem?


Ps: I'm new on MQX, and my board uses a DP83640 Transceiver.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,214 Views
Tgomes
Contributor III

Resolved, was a hardware problem. Thanks for the help

View solution in original post

0 Kudos
Reply
3 Replies
1,214 Views
sreejad
Contributor I

 Ethttool error:

       Cannot get settings:smileysurprised:peration not permitted.

This error is what I get when trying to get output of ethtool command with
different options in the freescale board MCF5485 with linux-2.6.29.What
could be the possible reason.

Sreeja

0 Kudos
Reply
1,214 Views
CarlFST60L
Senior Contributor II

Check the other thread I just posted in, works for me fine...

0 Kudos
Reply
1,215 Views
Tgomes
Contributor III

Resolved, was a hardware problem. Thanks for the help

0 Kudos
Reply