Ethernet link status

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,340件の閲覧回数
Tgomes
Contributor III

Hi everybody,

 

 

I'm trying to use the function "ipcfg_get_link_active" to figure out if an ethernet cable is connected or not, but it seems don't work as expected. The return is always true, even when the cable is unconnected. Is there any configuration that I can change or set for test and find the problem?


Ps: I'm new on MQX, and my board uses a DP83640 Transceiver.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,875件の閲覧回数
Tgomes
Contributor III

Resolved, was a hardware problem. Thanks for the help! 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,875件の閲覧回数
sreejad
Contributor I

 Ethttool error:

       Cannot get settings:smileysurprised:peration not permitted.

This error is what I get when trying to get output of ethtool command with
different options in the freescale board MCF5485 with linux-2.6.29.What
could be the possible reason.

Sreeja

0 件の賞賛
返信
1,875件の閲覧回数
CarlFST60L
Senior Contributor II

Check the other thread I just posted in, works for me fine...

0 件の賞賛
返信
1,876件の閲覧回数
Tgomes
Contributor III

Resolved, was a hardware problem. Thanks for the help! 

0 件の賞賛
返信