Ethernet link status

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Ethernet link status

跳至解决方案
2,412 次查看
Tgomes
Contributor III

Hi everybody,

 

 

I'm trying to use the function "ipcfg_get_link_active" to figure out if an ethernet cable is connected or not, but it seems don't work as expected. The return is always true, even when the cable is unconnected. Is there any configuration that I can change or set for test and find the problem?


Ps: I'm new on MQX, and my board uses a DP83640 Transceiver.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,947 次查看
Tgomes
Contributor III

Resolved, was a hardware problem. Thanks for the help! 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,947 次查看
sreejad
Contributor I

 Ethttool error:

       Cannot get settings:smileysurprised:peration not permitted.

This error is what I get when trying to get output of ethtool command with
different options in the freescale board MCF5485 with linux-2.6.29.What
could be the possible reason.

Sreeja

0 项奖励
回复
1,947 次查看
CarlFST60L
Senior Contributor II

Check the other thread I just posted in, works for me fine...

0 项奖励
回复
1,948 次查看
Tgomes
Contributor III

Resolved, was a hardware problem. Thanks for the help! 

0 项奖励
回复