Error installing MQX Eclipse plugin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error installing MQX Eclipse plugin

6,860 Views
tim_09
Contributor II

Hi,

i'm trying to install the MQX Eclipse plugin 4.0.2 for the DS-5 Vybrid Tower System Starter Kit Version 5.22.0 under Ubuntu 14.04 running in a virtual machine. During the installation process I get the error message you can see on the attached image.

Do I have the rigth plugin version? What can I do to solve this problem?

Thanks and best regards

Tim

0 Kudos
Reply
8 Replies

6,231 Views
tim_09
Contributor II

Hi Alejandro and Richard,

thanks for your help. Installing the plugin from the community in a clean install of DS-5 helped me solving this problem. Seems like everything works fine now.

Alejandro you could close the service request now as the solution solved the problem.

Thank you a lot. Great support.

Best regards

Tim

0 Kudos
Reply

6,231 Views
RossMcLuckie
NXP Employee
NXP Employee

Hi Alejandro,

Unfortunately I no longer support Vybrid, haven't done for quite some time, added richard_stulens​ who can hopefully help.

Thanks

Ross

0 Kudos
Reply

6,231 Views
alejandrolozan1
NXP Employee
NXP Employee

Got it Ross!!!

Thank you so much!

Alejandro

0 Kudos
Reply

6,231 Views
richard_stulens
NXP Employee
NXP Employee

Hi Alejandro,

We do not maintain that plugin anymore, but out engineer in the MQX team checked it anyway.

Here's his findings:

---

I’ve tried to install version of “MQX support” plug-in from this thread (https://community.freescale.com/thread/323233) into clean install of ARM DS-5 v5.22.0 (build: 5220021) under Ubuntu 14.04 and Windows7 without any problem and plug-ins works fine.

I would suggest to try install of plug-in again in clean DS-5 because “No repository found containing” problem makes no sense when all mentioned missing plug-ins are bundled in “MQX support.zip” file (which is in fact Eclipse update site containing these plug-ins).

---

Best regards,

Richard

6,231 Views
alejandrolozan1
NXP Employee
NXP Employee

Thanks Richard, I wil check it out!!!

/Alejandro

0 Kudos
Reply

6,231 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Have you checked this?

MQX4.1/tools/ds-5/ds5_update_site.zip updated and new name "MQX Support.zip"

MQX Plug-in not compatible with DS-5.18

Please try that plug-in and let me know how it goes.

/Alejandro

0 Kudos
Reply

6,231 Views
tim_09
Contributor II

Hi Alejandro,

thanks for your answer. Unfortunately installing this plugin generates a different error. error2.PNG

What could I do?

Regards,

Tim

0 Kudos
Reply

6,231 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

RossMcLuckie​, I hope you are doing well. Sorry to bother you but do you know it there is a problem with the MQX plug-in with version 5.22 of DS-5?

Is there someone that can provide a new plug-in?

Thanks a lot!!

Best Regards,

Alejandro

0 Kudos
Reply