Question about RAM for MPC5777C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question about RAM for MPC5777C

跳至解决方案
2,323 次查看
20Sidar04
Contributor III

Dear Mr./Mrs.,

I use MPC5777C.I would like find adress which reason of ECC error on RAM. How can I do this?
In addition to this question, does single bit error on RAM is corrected like FLASH? Finally,I would like to test RAM begin of programme. Walking 1 or Walking 0 test is only option test RAM. Or Does controller has hardware interface to do this test?

Best Regards.

标记 (2)
0 项奖励
回复
1 解答
2,311 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, use Error Reporting module (ERM) as in the example belows and/or machine check reporting registers:
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-1b-2b-RAM-ECC-error-injection-G...

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-1b-2b-FLASH-ECC-error-injection...


An application note for MPC5744P (it uses MEMU instead of ERM, in other aspects it may be similar, or documents describes all options):
https://www.nxp.com/docs/en/application-note/AN13179.pdf


As I know Walking ones/zeros test is not required, at least I haven't found any mentions in safety manual for this device.

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,312 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, use Error Reporting module (ERM) as in the example belows and/or machine check reporting registers:
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-1b-2b-RAM-ECC-error-injection-G...

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-1b-2b-FLASH-ECC-error-injection...


An application note for MPC5744P (it uses MEMU instead of ERM, in other aspects it may be similar, or documents describes all options):
https://www.nxp.com/docs/en/application-note/AN13179.pdf


As I know Walking ones/zeros test is not required, at least I haven't found any mentions in safety manual for this device.

 

0 项奖励
回复