Question about RAM for MPC5777C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about RAM for MPC5777C

Jump to solution
2,330 Views
20Sidar04
Contributor III

Dear Mr./Mrs.,

I use MPC5777C.I would like find adress which reason of ECC error on RAM. How can I do this?
In addition to this question, does single bit error on RAM is corrected like FLASH? Finally,I would like to test RAM begin of programme. Walking 1 or Walking 0 test is only option test RAM. Or Does controller has hardware interface to do this test?

Best Regards.

Tags (2)
0 Kudos
Reply
1 Solution
2,318 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, use Error Reporting module (ERM) as in the example belows and/or machine check reporting registers:
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-1b-2b-RAM-ECC-error-injection-G...

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-1b-2b-FLASH-ECC-error-injection...


An application note for MPC5744P (it uses MEMU instead of ERM, in other aspects it may be similar, or documents describes all options):
https://www.nxp.com/docs/en/application-note/AN13179.pdf


As I know Walking ones/zeros test is not required, at least I haven't found any mentions in safety manual for this device.

 

View solution in original post

0 Kudos
Reply
1 Reply
2,319 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, use Error Reporting module (ERM) as in the example belows and/or machine check reporting registers:
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-1b-2b-RAM-ECC-error-injection-G...

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-1b-2b-FLASH-ECC-error-injection...


An application note for MPC5744P (it uses MEMU instead of ERM, in other aspects it may be similar, or documents describes all options):
https://www.nxp.com/docs/en/application-note/AN13179.pdf


As I know Walking ones/zeros test is not required, at least I haven't found any mentions in safety manual for this device.

 

0 Kudos
Reply