Question about RAM for MPC5777C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about RAM for MPC5777C

ソリューションへジャンプ
2,322件の閲覧回数
20Sidar04
Contributor III

Dear Mr./Mrs.,

I use MPC5777C.I would like find adress which reason of ECC error on RAM. How can I do this?
In addition to this question, does single bit error on RAM is corrected like FLASH? Finally,I would like to test RAM begin of programme. Walking 1 or Walking 0 test is only option test RAM. Or Does controller has hardware interface to do this test?

Best Regards.

タグ(2)
0 件の賞賛
返信
1 解決策
2,310件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, use Error Reporting module (ERM) as in the example belows and/or machine check reporting registers:
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-1b-2b-RAM-ECC-error-injection-G...

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-1b-2b-FLASH-ECC-error-injection...


An application note for MPC5744P (it uses MEMU instead of ERM, in other aspects it may be similar, or documents describes all options):
https://www.nxp.com/docs/en/application-note/AN13179.pdf


As I know Walking ones/zeros test is not required, at least I haven't found any mentions in safety manual for this device.

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,311件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, use Error Reporting module (ERM) as in the example belows and/or machine check reporting registers:
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-1b-2b-RAM-ECC-error-injection-G...

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-1b-2b-FLASH-ECC-error-injection...


An application note for MPC5744P (it uses MEMU instead of ERM, in other aspects it may be similar, or documents describes all options):
https://www.nxp.com/docs/en/application-note/AN13179.pdf


As I know Walking ones/zeros test is not required, at least I haven't found any mentions in safety manual for this device.

 

0 件の賞賛
返信