How to determine the correct IGF module for WKUP_CH10 on MPC5746C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to determine the correct IGF module for WKUP_CH10 on MPC5746C

Jump to solution
1,105 Views
NileshDharap
Contributor III

Hello,
I’m working on the MPC5746C controller and need to enable the Input Glitch Filter (IGF) for Wakeup Channel 10 by setting the FGEN bit. However, since the device has 4 IGF modules, I’m unable to determine which IGF module corresponds to WKUP_CH10. I couldn't find a clear mapping in the reference manual

Could someone please help me identify which IGF module should be configured for WKUP_CH10?

Thank you in advance!

0 Kudos
Reply
1 Solution
1,074 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

IGF is being selected according attached I/O excel:

davidtosenovjan_0-1746787181765.png

davidtosenovjan_1-1746787199782.png

However this is not anyhow related to WKPU module. It has its own glithc filter being enabled by

davidtosenovjan_2-1746787268946.png

having following filtering behavior

davidtosenovjan_3-1746787285938.png

 

 

View solution in original post

0 Kudos
Reply
4 Replies
1,050 Views
NileshDharap
Contributor III

Hey David,

I was thinking IGF will be handling WKPU as well.
Thanks for the information.

Regards,
Nilesh Dharap

0 Kudos
Reply
1,075 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

IGF is being selected according attached I/O excel:

davidtosenovjan_0-1746787181765.png

davidtosenovjan_1-1746787199782.png

However this is not anyhow related to WKPU module. It has its own glithc filter being enabled by

davidtosenovjan_2-1746787268946.png

having following filtering behavior

davidtosenovjan_3-1746787285938.png

 

 

0 Kudos
Reply
798 Views
NileshDharap
Contributor III

Can you pls confirm that the implementation suggested above by enabling the register WKPU_WIFER on corresponding interrupt will meet the intention of requirement from safety manual i.e. Chapter 5.2.27 Glitch filter?

Tags (1)
0 Kudos
Reply
792 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Chapter '5.2.27 Glitch filter' only mentions the presence of glitch filters there, it does not say anything else and they can be used.

0 Kudos
Reply