Hello,
I’m working on the MPC5746C controller and need to enable the Input Glitch Filter (IGF) for Wakeup Channel 10 by setting the FGEN bit. However, since the device has 4 IGF modules, I’m unable to determine which IGF module corresponds to WKUP_CH10. I couldn't find a clear mapping in the reference manual
Could someone please help me identify which IGF module should be configured for WKUP_CH10?
Thank you in advance!
Solved! Go to Solution.
IGF is being selected according attached I/O excel:
However this is not anyhow related to WKPU module. It has its own glithc filter being enabled by
having following filtering behavior
Hey David,
I was thinking IGF will be handling WKPU as well.
Thanks for the information.
Regards,
Nilesh Dharap
IGF is being selected according attached I/O excel:
However this is not anyhow related to WKPU module. It has its own glithc filter being enabled by
having following filtering behavior
Can you pls confirm that the implementation suggested above by enabling the register WKPU_WIFER on corresponding interrupt will meet the intention of requirement from safety manual i.e. Chapter 5.2.27 Glitch filter?
Chapter '5.2.27 Glitch filter' only mentions the presence of glitch filters there, it does not say anything else and they can be used.