How to determine the correct IGF module for WKUP_CH10 on MPC5746C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to determine the correct IGF module for WKUP_CH10 on MPC5746C

跳至解决方案
956 次查看
NileshDharap
Contributor III

Hello,
I’m working on the MPC5746C controller and need to enable the Input Glitch Filter (IGF) for Wakeup Channel 10 by setting the FGEN bit. However, since the device has 4 IGF modules, I’m unable to determine which IGF module corresponds to WKUP_CH10. I couldn't find a clear mapping in the reference manual

Could someone please help me identify which IGF module should be configured for WKUP_CH10?

Thank you in advance!

0 项奖励
回复
1 解答
925 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

IGF is being selected according attached I/O excel:

davidtosenovjan_0-1746787181765.png

davidtosenovjan_1-1746787199782.png

However this is not anyhow related to WKPU module. It has its own glithc filter being enabled by

davidtosenovjan_2-1746787268946.png

having following filtering behavior

davidtosenovjan_3-1746787285938.png

 

 

在原帖中查看解决方案

0 项奖励
回复
4 回复数
901 次查看
NileshDharap
Contributor III

Hey David,

I was thinking IGF will be handling WKPU as well.
Thanks for the information.

Regards,
Nilesh Dharap

0 项奖励
回复
926 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

IGF is being selected according attached I/O excel:

davidtosenovjan_0-1746787181765.png

davidtosenovjan_1-1746787199782.png

However this is not anyhow related to WKPU module. It has its own glithc filter being enabled by

davidtosenovjan_2-1746787268946.png

having following filtering behavior

davidtosenovjan_3-1746787285938.png

 

 

0 项奖励
回复
649 次查看
NileshDharap
Contributor III

Can you pls confirm that the implementation suggested above by enabling the register WKPU_WIFER on corresponding interrupt will meet the intention of requirement from safety manual i.e. Chapter 5.2.27 Glitch filter?

标记 (1)
0 项奖励
回复
643 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Chapter '5.2.27 Glitch filter' only mentions the presence of glitch filters there, it does not say anything else and they can be used.

0 项奖励
回复