5748G USB example code ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

5748G USB example code ?

7,069件の閲覧回数
likai1929
Contributor II

I'm looking for some USB  example code. (I'm using the MPC 5748G)

I want USB0 to be device to send data to PC.Can you give some code?

thanks!

5 返答(返信)

6,282件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

Only available example is USB CDC-ECM demo application, which is part of SDK for MPC5748G.

This SDK is distributed with S32 Design Studio.

Please see the links below:

S32 Design Studio for Power Architecture 2017.R1 (Windows/Linux) released! 

S32 Design Studio for Power Architecture 2017.R1 - Update 8 available 

pastedImage_3.png

For more information about SDK stack, please see the document in the post attachment.

6,282件の閲覧回数
likai1929
Contributor II

thanks a lot.

  regards for you!

6,282件の閲覧回数
hassan_atyq
Contributor II

Hi Li Kai,

Please, do you have an example that makes USB communication ?

Thank you,
0 件の賞賛
返信

6,282件の閲覧回数
likai1929
Contributor II

Hi,

   I have touched the sample you told me, but I'm interested in USB working in device mode not host.

Can you show me more?

Thanks.

0 件の賞賛
返信

6,282件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

unfortunately the example I pointed you to is the only example available. If you need any other functionality, you will have to implement it on your own.

I am sorry for any inconvenience.

Regards,

Martin

0 件の賞賛
返信