******************************************************************************** * Detailed Description: * Application performs basic initialization, setup PLL to maximum allowed * frequency * * User can choose, which low power mode should be entered. There is LPU_MODE * macro defined, which allows to choose STOP, STANDBY or LPU_RUN mode. * * If LPU_RUN mode is selected, user can use macro LPU_STOP_SLEEP_STANDBY, * which allows to choose LPU_STOP, LPU_SLEEP or LPU_STANDBY mode. * * Ther is also RTC initialized, which wakeup microcontroller using WKPU after * 5 seconds from some of the LPU is entered. RTC uses FIRC as a source clock, * so FIRC must be enabled in all low power modes. * * * Modified files: mem.ld, sections.ld, startup.s, added file z2_restart.s * * * ------------------------------------------------------------------------------ * Test HW: MPC5748G-324DS, MPC574xG Motherboard * MCU: PPC5748GMMN6A 0N78S * Fsys: PLL0 160MHz * Debugger: Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * Target: internal_FLASH (debug mode, release mode) * EVB connection: USER LED1 to A1 * USER LED2 to A2 * * * ********************************************************************************
View full article