MCXA EVB cannot use linkserver to flash suddenly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCXA EVB cannot use linkserver to flash suddenly

ソリューションへジャンプ
1,170件の閲覧回数
Eason_L
Contributor III

Hi,

I use vscode to flash, and the ouput as below picture. How can I solve?

 

Eason_L_0-1723713547639.png

 

ラベル(2)
0 件の賞賛
返信
1 解決策
1,133件の閲覧回数
Eason_L
Contributor III

Hi Alice,

The problen is solved. I've ran below script and it can be flash with Segger setting.

Eason_L_0-1723797333118.png

Eason_L_1-1723797469306.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,139件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @Eason_L 

Thanks for your question.

Was it working properly before? If yes, How about entering ISP mode, then  erase full flash. 

If still can't work, please take a video or screenshots show your detail steps.

 

BR

Alice

0 件の賞賛
返信
1,134件の閲覧回数
Eason_L
Contributor III

Hi Alice,

The problen is solved. I've ran below script and it can be flash with Segger setting.

Eason_L_0-1723797333118.png

Eason_L_1-1723797469306.png

 

0 件の賞賛
返信