Cannot halt processor with EXT oscillator mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot halt processor with EXT oscillator mode

2,030 Views
limit1995
Contributor II

It is failed to set break point when debugging with following MCG configuration.

It run well without debugging.

 

const mcglite_config_t mcgliteConfig_BOARD_BootClockRUN =
    {
        .outsrc=kMCGLITE_ClkSrcExt,             /* MCGOUTCLK source is external clock source */
        .irclkEnableMode = MCG_IRCLK_DISABLE,     /* MCGIRCLK disabled */
        .ircs = kMCGLITE_Lirc8M,                  /* Slow internal reference (LIRC) 8 MHz clock selected */
        .fcrdiv = kMCGLITE_LircDivBy1,            /* Low-frequency Internal Reference Clock Divider: divided by 1 */
        .lircDiv2 = kMCGLITE_LircDivBy1,          /* Second Low-frequency Internal Reference Clock Divider: divided by 1 */
        .hircEnableInNotHircMode = false,         /* HIRC source is not enabled */
    };

 

Error report

limit1995_0-1735205073255.png

My board is FRDM-MCXC242.

How to deal with the problem?

 

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

2,005 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @limit1995 

Could you please show me where you set the breakpoint? And which demo did you use? I will help to check on my side. Thank you.

BR

Alice

0 Kudos
Reply

1,967 Views
limit1995
Contributor II

Dear @Alice_Yang 

I set the clock configuration based on demo app led_blinky.

limit1995_3-1735526998497.png

Then update the source files.

limit1995_4-1735527054075.png

And step-by-step dubugging caused error like below.

limit1995_5-1735527212850.png

 

The part of the automatically generated clock_config.c is as follows:

void BOARD_InitBootClocks(void)
{
    BOARD_BootClockRUN();
}

/*******************************************************************************
 ********************** Configuration BOARD_BootClockRUN ***********************
 ******************************************************************************/
/* clang-format off */
/* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
!!Configuration
name: BOARD_BootClockRUN
called_from_default_init: true
outputs:
- {id: Bus_clock.outFreq, value: 16.384 kHz}
- {id: Core_clock.outFreq, value: 32.768 kHz}
- {id: ERCLK32K.outFreq, value: 32.768 kHz}
- {id: Flash_clock.outFreq, value: 16.384 kHz}
- {id: LPO_clock.outFreq, value: 1 kHz}
- {id: MCGIRCLK.outFreq, value: 8 MHz}
- {id: MCGPCLK.outFreq, value: 48 MHz}
- {id: OSCERCLK.outFreq, value: 32.768 kHz}
- {id: System_clock.outFreq, value: 32.768 kHz}
settings:
- {id: MCGMode, value: EXT}
- {id: MCG.CLKS.sel, value: SIM.OSCCLK}
- {id: MCG_C2_OSC_MODE_CFG, value: ModeOscLowPower}
- {id: MCG_MC_HIRCEN_CFG, value: Enabled}
- {id: OSC0_CR_ERCLKEN_CFG, value: Enabled}
- {id: OSC_CR_ERCLKEN_CFG, value: Enabled}
- {id: OSC_CR_SYS_OSC_CAP_LOAD_CFG, value: SC12PF}
- {id: SIM.CLKOUTSEL.sel, value: MCG.MCGPCLK}
- {id: SIM.COPCLKSEL.sel, value: OSC.OSCERCLK}
- {id: SIM.FLEXIOSRCSEL.sel, value: MCG.MCGPCLK}
- {id: SIM.LPUART0SRCSEL.sel, value: MCG.MCGPCLK}
- {id: SIM.LPUART1SRCSEL.sel, value: MCG.MCGPCLK}
- {id: SIM.RTCCLKOUTSEL.sel, value: OSC.OSCERCLK}
- {id: SIM.TPMSRCSEL.sel, value: MCG.MCGPCLK}
- {id: SIM.USBSRCSEL.sel, value: MCG.MCGPCLK}
sources:
- {id: MCG.HIRC.outFreq, value: 48 MHz}
- {id: OSC.OSC.outFreq, value: 32.768 kHz, enabled: true}
 * BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS **********/
/* clang-format on */

/*******************************************************************************
 * Variables for BOARD_BootClockRUN configuration
 ******************************************************************************/
const mcglite_config_t mcgliteConfig_BOARD_BootClockRUN =
    {
        .outsrc=kMCGLITE_ClkSrcExt,             /* MCGOUTCLK source is external clock source */
        .irclkEnableMode = kMCGLITE_IrclkEnable,  /* MCGIRCLK enabled, MCGIRCLK disabled in STOP mode */
        .ircs = kMCGLITE_Lirc8M,                  /* Slow internal reference (LIRC) 8 MHz clock selected */
        .fcrdiv = kMCGLITE_LircDivBy1,            /* Low-frequency Internal Reference Clock Divider: divided by 1 */
        .lircDiv2 = kMCGLITE_LircDivBy1,          /* Second Low-frequency Internal Reference Clock Divider: divided by 1 */
        .hircEnableInNotHircMode = true,          /* HIRC source is enabled */
    };
const sim_clock_config_t simConfig_BOARD_BootClockRUN =
    {
        .er32ksrc=SIM_OSC32KSEL_OSC32KCLK_CLK,  /* OSC32KSEL select: OSC32KCLK clock */
        .clkdiv1 = 0x10000U,                      /* SIM_CLKDIV1 - OUTDIV1: /1, OUTDIV4: /2 */
    };
const osc_config_t oscConfig_BOARD_BootClockRUN =
    {
        .freq = 32768U,                           /* Oscillator frequency: 32768Hz */
        .capLoad = (kOSC_Cap4P | kOSC_Cap8P),     /* Oscillator capacity load: 12pF */
        .workMode = kOSC_ModeOscLowPower,         /* Oscillator low power */
        .oscerConfig =
            {
                .enableMode = kOSC_ErClkEnable,   /* Enable external reference clock, disable external reference clock in STOP mode */
            }
    };

/*******************************************************************************
 * Code for BOARD_BootClockRUN configuration
 ******************************************************************************/
void BOARD_BootClockRUN(void)
{
    /* Set the system clock dividers in SIM to safe value. */
    CLOCK_SetSimSafeDivs();
    /* Initializes OSC0 according to board configuration. */
    CLOCK_InitOsc0(&oscConfig_BOARD_BootClockRUN);
    CLOCK_SetXtal0Freq(oscConfig_BOARD_BootClockRUN.freq);
    /* Set MCG to EXT mode. */
    CLOCK_SetMcgliteConfig(&mcgliteConfig_BOARD_BootClockRUN);
    /* Set the clock configuration in SIM module. */
    CLOCK_SetSimConfig(&simConfig_BOARD_BootClockRUN);
    /* Set SystemCoreClock variable. */
    SystemCoreClock = BOARD_BOOTCLOCKRUN_CORE_CLOCK;
}

 

 

0 Kudos
Reply

1,949 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @limit1995 

In MCG control register 1, it changes the clock source for the main clock. It cannot be debugged when the clock source is changed.

 

BR

Alice

0 Kudos
Reply

1,933 Views
limit1995
Contributor II

Dear @Alice_Yang ,

It is ok to step-over BOARD_InitBootClocks() with HIRC mode.

But it is failed to step-over BOARD_InitBootClocks() or to set break point with EXT mode. Debugging is not possible at all.

Why?

And I want to know how to debug with EXT mode.

 

Thanks.

0 Kudos
Reply