The table below contains notable updates to the current release of the Reference Manual. The information provided here is preliminary and subject to change without notice.
Affected Modules
Issue Summary
Description
Date
MCXNx4x Pinout xlsx Attachment
Defeature PF* pins
Erroneous pinouts to PF* signals on ALT11 are removed. Before: joseph_hernandez_0-1709937861704.png
After:
joseph_hernandez_1-1709937951033.png
01 March 2024
System Boot ROM API
Missing Boot Modes sections in ROM API chapter of System Boot
New sections added:
15.3 Boot modes
15.3.1 Master boot mode
Master boot mode supports the following boot devices:
Internal flash memory boot
FlexSPI NOR flash memory boot
SPI 1-bit NOR recovery boot
Secondary bootloader boot
Table 229. Image offsets for different boot media
Boot media
Image offset
Internal flash memory boot
0h
FlexSPI NOR flash memory boot
1000h
SPI 1-bit NOR recovery boot
0h
Secondary bootloader boot
0h
15.3.2 Secondary bootloader mode
The Secondary bootloader mode can be enabled by setting the CMPA[BOOT_SRC] as 2, the image loaded in the Bank1_IFR0 region (0x0100_8000 to 0x0100_FFFF) will be set as primary boot mode, and the secondary boot image will boot first after the device reset. The secondary boot image type can be plain, crc or signed image, but cannot set as the SB file.
Based on the CMPA[OEM_BANK1_IFR0_PROT](0x01004004[5:7]) setting, after the secondary boot image boot, the Bank1_IFR0 region will be configured with different MBC setting:
Lifecycle
CMPA[OEM_BANK1_IFR0_PROT]
Secondary bootloader mode MBC
IFR0 recovery boot MBC
Develop (0x3)
NA
GLABC0
GLBAC0
Develop2 (0x7), In-field (0xF), In-field Locked (0xCF), Field Return OEM (1F)
0
GLBAC4
GLBAC4
1
GLBAC4
2
GLBAC2
3
GLBAC6
4
GLBAC4
5
6
7
01 March 2024
Input Multiplexing (INPUTMUX)
Clarification to CMP trigger input registers
Update to the CMPx_TRIG Register function description for the following registers: CMP0_TRIG (260h), CMP1_TRIG (4EOh), and CMP2_TRIG (500h) Before:
Function
This register selects the CMPx trigger inputs
After:
Function
This register selects the CMPx SAMPLE/WINDOW input
01 March 2024
記事全体を表示