SDK 2.6.2 MIMXRT1061xxxxA FreeRTOS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK 2.6.2 MIMXRT1061xxxxA FreeRTOS

Jump to solution
1,490 Views
MartinHo
Contributor IV

When configuring the i.MX RT1061 SDK it's possible to select FreeRTOS as OS, but when I try to create a New project I can not select the FreeRTOS as component (while this is possible when i select the i-MX RT1062). Is this an error or a limit of the RT1061?

Martin

0 Kudos
Reply
1 Solution
1,299 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Martin:

Currently Amazon freeRTOS in SDK is board dependent. Since we don't have an EVK board based on RT1061, this option is not enabled.  This is not an limitation of RT1061.

We will enable the freeRTOS on all supported devices in future.

Regards

Daniel

View solution in original post

0 Kudos
Reply
1 Reply
1,300 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Martin:

Currently Amazon freeRTOS in SDK is board dependent. Since we don't have an EVK board based on RT1061, this option is not enabled.  This is not an limitation of RT1061.

We will enable the freeRTOS on all supported devices in future.

Regards

Daniel

0 Kudos
Reply