SDK 2.6.2 MIMXRT1061xxxxA FreeRTOS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK 2.6.2 MIMXRT1061xxxxA FreeRTOS

ソリューションへジャンプ
1,703件の閲覧回数
MartinHo
Contributor IV

When configuring the i.MX RT1061 SDK it's possible to select FreeRTOS as OS, but when I try to create a New project I can not select the FreeRTOS as component (while this is possible when i select the i-MX RT1062). Is this an error or a limit of the RT1061?

Martin

0 件の賞賛
返信
1 解決策
1,512件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Martin:

Currently Amazon freeRTOS in SDK is board dependent. Since we don't have an EVK board based on RT1061, this option is not enabled.  This is not an limitation of RT1061.

We will enable the freeRTOS on all supported devices in future.

Regards

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,513件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Martin:

Currently Amazon freeRTOS in SDK is board dependent. Since we don't have an EVK board based on RT1061, this option is not enabled.  This is not an limitation of RT1061.

We will enable the freeRTOS on all supported devices in future.

Regards

Daniel

0 件の賞賛
返信