SDK 2.6.2 MIMXRT1061xxxxA FreeRTOS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SDK 2.6.2 MIMXRT1061xxxxA FreeRTOS

跳至解决方案
1,705 次查看
MartinHo
Contributor IV

When configuring the i.MX RT1061 SDK it's possible to select FreeRTOS as OS, but when I try to create a New project I can not select the FreeRTOS as component (while this is possible when i select the i-MX RT1062). Is this an error or a limit of the RT1061?

Martin

0 项奖励
回复
1 解答
1,514 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Martin:

Currently Amazon freeRTOS in SDK is board dependent. Since we don't have an EVK board based on RT1061, this option is not enabled.  This is not an limitation of RT1061.

We will enable the freeRTOS on all supported devices in future.

Regards

Daniel

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,515 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi Martin:

Currently Amazon freeRTOS in SDK is board dependent. Since we don't have an EVK board based on RT1061, this option is not enabled.  This is not an limitation of RT1061.

We will enable the freeRTOS on all supported devices in future.

Regards

Daniel

0 项奖励
回复