SDK 2.4 Debug issue se_hosthib_exemples aws_jitr_demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDK 2.4 Debug issue se_hosthib_exemples aws_jitr_demo

1,438件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

Hello guys,

I got an issue since the switch to SDK 2.4 project. For now I was using the exemples released in A71CH Software Package. I heard that it was integrated onto SDK 2.4 so I imported the project with MCUXpresso 10.2.

My issue is that when starting the project an HardFault_Handler pop out at the start of the scheduler of FreeRTOS.

I didn't touch anything. I'm runnign it on a FRDM-K64F rev E board with the A71CH arduino compatible shield OM3710/A71CHARD.

pastedImage_1.png

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,313件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Theophile Leroy

Do you have errors just in those 2 example codes? Using the same SDK and IDE that you have, I have tried them in my frdm-K64F SCH-REV-D1  and I don't see any problem in them. I will try to use the exact Schematic revision that you have and if I find something I will let you know.

Best regards

Jorge Alcala

1,313件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

Ok solved the issue by switching to SDK 2.4.1. Project is working fine on this one. I don't know where the error come form... Maybe not a big deal.

Thank you for help

0 件の賞賛
返信