SDK 2.4 Debug issue se_hosthib_exemples aws_jitr_demo

cancel
Showing results for 
Search instead for 
Did you mean: 

SDK 2.4 Debug issue se_hosthib_exemples aws_jitr_demo

227 Views
theophileleroy
NXP Employee
NXP Employee

Hello guys,

I got an issue since the switch to SDK 2.4 project. For now I was using the exemples released in A71CH Software Package. I heard that it was integrated onto SDK 2.4 so I imported the project with MCUXpresso 10.2.

My issue is that when starting the project an HardFault_Handler pop out at the start of the scheduler of FreeRTOS.

I didn't touch anything. I'm runnign it on a FRDM-K64F rev E board with the A71CH arduino compatible shield OM3710/A71CHARD.

pastedImage_1.png

Labels (1)
0 Kudos
2 Replies

102 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Theophile Leroy

Do you have errors just in those 2 example codes? Using the same SDK and IDE that you have, I have tried them in my frdm-K64F SCH-REV-D1  and I don't see any problem in them. I will try to use the exact Schematic revision that you have and if I find something I will let you know.

Best regards

Jorge Alcala

102 Views
theophileleroy
NXP Employee
NXP Employee

Ok solved the issue by switching to SDK 2.4.1. Project is working fine on this one. I don't know where the error come form... Maybe not a big deal.

Thank you for help

0 Kudos