BLE Device name Error[N/A] using example code of [HRS] <KW38 EVB>

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BLE Device name Error[N/A] using example code of [HRS] <KW38 EVB>

ソリューションへジャンプ
2,712件の閲覧回数
JungkyuHan1
Contributor III

Hello

 

I am using the device #KW38 EVB

When I test with two example code; <heart rate sensor>,<blood pressure sensor>, I found some difference of SCAN result.

(I tested with SAMSUNG Galaxy Note 9 phone)

Using <blood pressure sensor> , the [Device Name] in host is always [NXP_BPS]. Exaclty I expected.

BUT, Using <heart rate sensor> , the [Device Name] in host is always [N/A]. I expected [NXP_HRS]. 

 

I have No idea what makes this diffence. Anybody can explain this and how to fix the fault scanning result?

 

 

 

JungkyuHan1_2-1684722687224.png

 

HRS_NA_01.jpgNXP_BPS_01.jpg

0 件の賞賛
返信
1 解決策
2,634件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Did you modify the source code of any of those examples?

What is the android version of your android device? Can you test these applications with a newer android version?

You mention that you tested other projects, and the same issue occurs, could you please confirm if you observed this behavior using the IoT Toolbox App?

Regards,
Eduardo.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,694件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @JungkyuHan1

Hope you are doing well.

What SDK version are you using? Please try using the latest SDK version.

By any chance, did you modify the source code of any of those examples?

Have you previously paired the FRDM-KW38 with your mobile device (perhaps using another BLE example project)? If so, please try removing the Bluetooth pairing data/paired devices from your mobile device.

Also, could you please confirm if the same behavior is observed using the IoT Toolbox App?

EduardoZamora_1-1684776222779.pngEduardoZamora_0-1684776222776.png

Regards,
Eduardo.

0 件の賞賛
返信
2,688件の閲覧回数
JungkyuHan1
Contributor III
Dear Eduardo. Thankyou for your advise.
<SDK Info>
This is SDK version 2.6.615 manifest file. It describes the content of the FRDM-KW38 and additional settings for tools that support SDK version 2.6.615
ID:SDK_2.x_FRDM-KW38
Name:FRDM-KW38
Timestamp (UTC): 2023-02-23 14:33:08.853680

============================================
I Tested other example projects. Two of the projects <Heart rate sensor/BLE Shell> are shown the same symtom. The others are FINE.

1. Cycling Power Sensor[NXP_CPS]
2. Glucose Sensor[NXP_GLS]
3. Health thermometer[NXP_HTS]
4. Heart Rate Sensor [N/A] <====== Error
5. Proximity reporter[NXP_PXR]
6. Running speed cadence sensor[NXP_RSCS]
7. Wireless uart[NXP_WU]
8. Ble_Shell [N/A] <====== Error
0 件の賞賛
返信
2,635件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Did you modify the source code of any of those examples?

What is the android version of your android device? Can you test these applications with a newer android version?

You mention that you tested other projects, and the same issue occurs, could you please confirm if you observed this behavior using the IoT Toolbox App?

Regards,
Eduardo.

0 件の賞賛
返信