BLE Device name Error[N/A] using example code of [HRS] <KW38 EVB>

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

BLE Device name Error[N/A] using example code of [HRS] <KW38 EVB>

跳至解决方案
2,506 次查看
JungkyuHan1
Contributor II

Hello

 

I am using the device #KW38 EVB

When I test with two example code; <heart rate sensor>,<blood pressure sensor>, I found some difference of SCAN result.

(I tested with SAMSUNG Galaxy Note 9 phone)

Using <blood pressure sensor> , the [Device Name] in host is always [NXP_BPS]. Exaclty I expected.

BUT, Using <heart rate sensor> , the [Device Name] in host is always [N/A]. I expected [NXP_HRS]. 

 

I have No idea what makes this diffence. Anybody can explain this and how to fix the fault scanning result?

 

 

 

JungkyuHan1_2-1684722687224.png

 

HRS_NA_01.jpgNXP_BPS_01.jpg

0 项奖励
回复
1 解答
2,428 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Did you modify the source code of any of those examples?

What is the android version of your android device? Can you test these applications with a newer android version?

You mention that you tested other projects, and the same issue occurs, could you please confirm if you observed this behavior using the IoT Toolbox App?

Regards,
Eduardo.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,488 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @JungkyuHan1

Hope you are doing well.

What SDK version are you using? Please try using the latest SDK version.

By any chance, did you modify the source code of any of those examples?

Have you previously paired the FRDM-KW38 with your mobile device (perhaps using another BLE example project)? If so, please try removing the Bluetooth pairing data/paired devices from your mobile device.

Also, could you please confirm if the same behavior is observed using the IoT Toolbox App?

EduardoZamora_1-1684776222779.pngEduardoZamora_0-1684776222776.png

Regards,
Eduardo.

0 项奖励
回复
2,482 次查看
JungkyuHan1
Contributor II
Dear Eduardo. Thankyou for your advise.
<SDK Info>
This is SDK version 2.6.615 manifest file. It describes the content of the FRDM-KW38 and additional settings for tools that support SDK version 2.6.615
ID:SDK_2.x_FRDM-KW38
Name:FRDM-KW38
Timestamp (UTC): 2023-02-23 14:33:08.853680

============================================
I Tested other example projects. Two of the projects <Heart rate sensor/BLE Shell> are shown the same symtom. The others are FINE.

1. Cycling Power Sensor[NXP_CPS]
2. Glucose Sensor[NXP_GLS]
3. Health thermometer[NXP_HTS]
4. Heart Rate Sensor [N/A] <====== Error
5. Proximity reporter[NXP_PXR]
6. Running speed cadence sensor[NXP_RSCS]
7. Wireless uart[NXP_WU]
8. Ble_Shell [N/A] <====== Error
0 项奖励
回复
2,429 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Did you modify the source code of any of those examples?

What is the android version of your android device? Can you test these applications with a newer android version?

You mention that you tested other projects, and the same issue occurs, could you please confirm if you observed this behavior using the IoT Toolbox App?

Regards,
Eduardo.

0 项奖励
回复