Restart Button enable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Restart Button enable

Jump to solution
57,389 Views
claudiobrunelli
Contributor II

In the debug perspective I can't use the restart button, due to fact it's not enabled.

But in the customized perspective it's still enabled. There is something different to set ?

1 Solution
56,172 Views
Toe
Contributor IV

I had the same problem on a couple new projects.  I think the problem happens when the debug configuration is created.  I tried a few things and found if I remove this line from the .launch file the restart button becomes active:

<stringAttribute key="org.eclipse.cdt.launch.DEBUGGER_START_MODE" value="remote"/>

Give that a try, maybe it will help you as well.

View solution in original post

41 Replies
37,214 Views
lpcxpresso_supp
NXP Employee
NXP Employee

So far, we've been unable to reproduce the problem. However, a small refactoring that included the Restart toolbar/button has been done for the upcoming v11.1.0 release.

pastedImage_1.png

Greetings,
MCUXpresso IDE Support

0 Kudos
Reply
36,911 Views
claudiobrunelli
Contributor II

I'm sorry I don't want to be heavvy but the restart button doesn't work yet.

Now we are 3 people using mcuxpresso but this kind of push button doesn't work.

3 different collegue, 3 different pc, same problem !!!

We can't use the restart button, it is still light gray !

How it's possible. May be something wrong wit os ? Perhaps there is a special set to be done with configuration ?

It's not so confortable to reload every time the prject.

Thanks...Claudio

 

0 Kudos
Reply
36,676 Views
ErichStyger
Specialist I

Hi @claudiobrunelli ,

can you check if Terminate & Relaunch

ErichS_0-1605546573374.pngErichS_0-1605546573374.png

 

Works for you?

Erich

0 Kudos
Reply
36,651 Views
claudiobrunelli
Contributor II

Hi guys, thanks for your help.

Yes Erich I tried with terminate & launch. But the button is still disabled.

I'd like to test the Toe's proposal but where is that file ? Is it in the project path ?

 

Thanks.

Claudio

0 Kudos
Reply
36,643 Views
ErichStyger
Specialist I

It is present in the .launch configuration file you are using. Open the .launch inside your project with a text editor or inside Eclipse

ErichS_0-1605629913914.pngErichS_0-1605629913914.png

 

0 Kudos
Reply
36,649 Views
Toe
Contributor IV

By default it is in the workspace directory:

workspace\.metadata\.plugins\org.eclipse.debug.core\.launches

But you can also make it a file that is local to the project by going to the debug configuration, Common tab, and select "Shared File"

0 Kudos
Reply
36,678 Views
ErichStyger
Specialist I

Just in case, if the .launch is somehow screwed up: delete it (better: make a backup to see the difference later) and it will be recreated from scratch. Maybe that cures the problem?

0 Kudos
Reply
56,173 Views
Toe
Contributor IV

I had the same problem on a couple new projects.  I think the problem happens when the debug configuration is created.  I tried a few things and found if I remove this line from the .launch file the restart button becomes active:

<stringAttribute key="org.eclipse.cdt.launch.DEBUGGER_START_MODE" value="remote"/>

Give that a try, maybe it will help you as well.

35,860 Views
paolocolombo
Contributor III

Good morning everyone,

I have successfully followed the instructions to enable the reset button with the MCUXpresso 11.3 version. Now I have updated my system with version 11.4 and the solution to delete the line in the .launch file no longer works, because every time I launch the debugger the .launch file is re-created with the line in question present. How can I fix the problem again?

Tags (1)
0 Kudos
Reply
35,829 Views
lpcxpresso_supp
NXP Employee
NXP Employee

@claudiobrunelli @paolocolombo @Toe 

First of all, manual changes inside the IDE-managed launch configuration are completely discouraged... Users indirectly change its contents by interacting with the Debug Configurations section. Manual changes can have nasty side-effects as well.

@Toe - would you please explain how did you conclude that "DEBUGGER_START_MODE" is the attribute that must be removed?

We would also need the following details from anyone experiencing the described issue:

  1. What IDE version?
  2. What MCU/board?
  3. What type of project (e.g. SDK-based)?
  4. Is the problem reproducible with a 'hello world' project from SDK
  5. What SDK version?
  6. What debug solution (e.g. LinkServer, PEmicro, J-Link)?
  7. Is a debug session on some other probe type exhibiting the same problem?
  8. If PEmicro/J-Link is used, are these software packages changed/updated compared to what the IDE is shipped with?
  9. How is the launch configuration created?
  10. If using the 'blue debug' button (see ch. 11.1.1 from User Guide), is the problem still reproducible?
  11. Attach here the problematic launch configurations.

I also noticed in the previous posts that "workspace\.metadata\.plugins\org.eclipse.debug.core\.launches" was referred as the placeholder for created launch configurations. If this is the case, then this is a potential sign that launch configurations are manually created instead of using the 'blue debug' button (see ch. 11.1.1 from User Guide). The launch configurations should be inside the project. Manually created launch configuration might have incorrectly attributes set (e.g. "DEBUGGER_START_MODE").

Please help with the above information. Maybe if we have the requested data, we can try a blind fix at some point... 

Greetings,
MCUXpresso IDE Support

 

 

0 Kudos
Reply
35,772 Views
Toe
Contributor IV

I found the problem by doing a diff between different .launch files. I had a few that did have the restart button active and some that didn't. I tried a few options before narrowing in that the DEBUGGER_START_MODE tag was the culprit in the non-working launch and removing it 

1.) I'm currently using 11.4 and 11.3.1, but have seen it in versions prior to these.

2.) K22, KL17, K40, K60, and K12 MCUs using custom boards.

3.) SDK based project.

4.) Yes. To provide additional details I just created a K64 project using SDK 2.8.2 for the FRDM K64 board. I did not add any additional drivers or code. The SDA connection on my FRDM board is setup to use the PEMicro OpenSDA firmware.  I have attached the .launch file generated, debugging with this file does have the "restart" button greyed out. By taking the same file and removing the line in question, that button comes back after restarting the IDE.

5.) SDK version does not matter for the MCUs listed, but see #4.

6.) PEMicro

7.) I have seen this with OpenSDA and the PEMicro multilinks. I do not recall seeing it with Segger OpenSDA or J-Link, but those are not the most used solutions for us.

8.) No, the drivers from the IDE are what is being used.

9.) I usually create my launch configurations by going to the debug configurations screen and double clicking on the interface I intend to use. This generates a basic configuration that I can edit. By default these are set to be saved as a "local" file which lives in the workspace dir for the IDE; this can be changed to a "shared" file and is easier to find. This method of generation obviously does things different than the blue button method.

10.) No, the file generated that way does not have the broken line.

11.) The file is attached.

It seems that the debug configuration manager needs to use the same method of generating the .launch file as the blue button from the quickstart panel. That configuration manager is the way files are accessed or modified after they are created anyway.

0 Kudos
Reply
35,767 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Thanks a lot. This is valuable information. So long story short, only manually created PEmicro debug configurations cause the described behavior. Now that we narrowed down the problem, we'll try to reproduce it on our side.

 

It seems that the debug configuration manager needs to use the same method of generating the .launch file as the blue button from the quickstart panel. That configuration manager is the way files are accessed or modified after they are created anyway.

Creating launch configurations the way you described (i.e. double-clicking the debug solution type) is not something that is completely under our control, thus some differences with regards to the attributes added in the launch configuration. The UG chapter I mentioned in my previous post even has an important note that's related to what I've just written (see screenshot below).

lpcxpresso_supp_0-1631025996336.pnglpcxpresso_supp_0-1631025996336.png

 

Given current data, I recommend using the blue debug button for starting a debug session, as described in the User Guide. Once the debug configuration is created this way, it can be further changed as needed.

Greetings,
MCUXpresso IDE Support

0 Kudos
Reply
35,852 Views
myke_predko
Senior Contributor III

@paolocolombo 

I had a lot of problems with transitioning from 11.3.1 to 11.4.0 - one of the biggies is that the workspace is not compatible between the versions.  

If you're using the same workspace, then I recommend that you create a new one and recreate your projects in there.  It was suggested that you can drag and drop the projects between workspaces but I think it's safer to bring in the source and create a new project in the workspace.  

Good luck!

0 Kudos
Reply
36,555 Views
claudiobrunelli
Contributor II

Hi Toe, Hi Erich.

My apologies for late reply.

I didn't try till today yours suggestions. Now, finally, the restart button works properly. It's not enought to delete the .launch files and recreate it. The the string attribute key DEBUGGER_START_MODE, must be removed too from file otherwise the button is always locked.

Thanks a lot.

Claudio

 

Tags (1)
0 Kudos
Reply
36,680 Views
ErichStyger
Specialist I

That's an interesting route.

But I do have this

<stringAttribute key="org.eclipse.cdt.launch.DEBUGGER_START_MODE" value="remote"/>

present in my launch files and the restart button is enable too.

Curious how removing it would trigger something different?

But worth a try for sure, let us know.

0 Kudos
Reply
36,748 Views
ErichStyger
Specialist I

Hi @claudiobrunelli ,

could you share a screenshot and the version/host you are on by now?

I'm on Win10 64 J-Link and on 11.2.1 and I can tell it works for me:

ErichS_0-1604413559323.pngErichS_0-1604413559323.png

 

Few ideas what could cause this:

- did you try with a fresh/new workspace too?

- reset the perspective(s)?

- did you had the 'Quickstart' view open/active: this one seems to have an impact on the debug icons, so make sure it is shown at least once.

 

I hope this helps,

Erich

0 Kudos
Reply
36,741 Views
claudiobrunelli
Contributor II

Hi Erich

I'm using a window 10 PRO, just a freedom board based on KE16 (but I did the same problem on K27 and a factory target too) and the system debug was at the beginning the open SDA than now a Universal multilink of PEMicro.

But it's still doesn't work this button. My collegues too, have the same problem. If you need other info I can give it of course.

Thanks in advance, Claudio

 

 

   

 

0 Kudos
Reply
36,748 Views
ErichStyger
Specialist I

Hi @claudiobrunelli ,

which IDE/version?

I'm on V11.2.1 (https://mcuoneclipse.com/2020/10/17/mcuxpresso-ide-v11-2-1/ ) and I can say that it works there for me (Win10 64bit, mostly using Kinetis and LPC parts):

ErichS_0-1604412762112.pngErichS_0-1604412762112.png

I had issues in the past too, and this is what helped me:

- try with a fresh/new workspace: When I did too much toolbar customization I faced some issues

- make sure that the Quickstart view is loaded/visible. E.g. switch to the 'Develop' perspective to see if this helps

 

Any other details you could share would be helpful to find out what is missing or different on your end.

 

I hope this helps,

Erich

0 Kudos
Reply
36,994 Views
claudiobrunelli
Contributor II

I take note about your answer. Just to clarify than, I send you other screenshot where there's my xpresso release.
If you have news about this strange problem, please advice me. Thanks a lot.

Claudio

pastedImage_3.pngpastedImage_5.png

0 Kudos
Reply
36,750 Views
lpcxpresso_supp
NXP Employee
NXP Employee

It should be enabled. Please note that its enablement depends on the currently selected context from Debug view. In other words, you'll have to select the thread or the main process, not the top-level item associated with the debug configuration.

Greetings,
MCUXpresso IDE Support

0 Kudos
Reply
36,692 Views
ErichStyger
Specialist I

The screenshot actually shows that a context (and not the top level item) is selected, and the restart button is disabled. So imho this is caused by this.

I thought it might be related to the P&E debug probe, but I have it working on my side (just checked again) (see my screenshot). So all good there (using K22)

I don't have a KE device so not sure if this is related to the device or not.

I hope this helps,

Erich

 
 
 
 

 

 

0 Kudos
Reply