Refresh automatically before build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Refresh automatically before build

ソリューションへジャンプ
5,372件の閲覧回数
kensu
Contributor V

Hi,

For MCUXpresso, how to refresh automatically every time before build?

Because I don't want to refresh manually the project while I add a source code file.

Thanks

Ken

タグ(2)
0 件の賞賛
返信
1 解決策
5,180件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信
6 返答(返信)
5,180件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

How exactly are you adding new source files? If you create new files within the IDE itself, or drag'n'drop files from Windows Explorer (etc) into the project inside the IDE's Project Explorer view - then the new files should automatically be detected.

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信
5,180件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I believe his problem case is that the extra file(s) are created outside the IDE, and that way the IDE is not aware it and does not included.

Erich

0 件の賞賛
返信
5,180件の閲覧回数
kensu
Contributor V

Hi Erich

Yes, sometimes, team members may add source code outside IDE (ex: SVN), so I want to know how to set.

Thanks for your support, I will wait.

Ken

0 件の賞賛
返信
5,181件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Ken,

hopefully this is what you are looking for:

Automatically Refresh Eclipse Projects before Build | MCU on Eclipse 

?

Erich

0 件の賞賛
返信
5,180件の閲覧回数
kensu
Contributor V

Hi Erich

Thanks a lot.

This article solved my problem.

Ken

0 件の賞賛
返信
5,181件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Ken,

I solved that problem in the past and solved it with a custom builder. I would need some time tonight to write it up. I hope it can wait for a few hours.

Erich

0 件の賞賛
返信