I can not program file into flash by MCUXpressIDE, here is some log about this situation,
ProgramPage (0x10000000, 0x2208, 0x4000) status 0x1 - driver reported driver error - EXTSPI driver rc 128 (0x80)
Closing flash driver LPC540xx_SPIFI_SFDP.cfx
(100) Writing Flash ended with an error.
File 'lpcxpresso54018_touch_cursor.axf' load failure: Ef(49): Flash driver operation gave error.
(100) Target Connection Failed
Unable to perform operation!
Command failed with exit code 1
how can I slove this problem ?
已解决! 转到解答。
Hi,
Could you please let me know which project are you using?, please try placing the MCU in ISP mode and then try launching the debug session, you can find more information on this link:
Regaining debug access to target MCU
Hope it helps!
Regards
Soledad
Hi,
Could you please let me know which project are you using?, please try placing the MCU in ISP mode and then try launching the debug session, you can find more information on this link:
Regaining debug access to target MCU
Hope it helps!
Regards
Soledad