I can not program file into flash by MCUXpressIDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I can not program file into flash by MCUXpressIDE

Jump to solution
1,913 Views
seamas
Contributor I

I can not program file into flash by MCUXpressIDE, here is some log about this situation,

ProgramPage (0x10000000, 0x2208, 0x4000) status 0x1 - driver reported driver error - EXTSPI driver rc 128 (0x80)
Closing flash driver LPC540xx_SPIFI_SFDP.cfx
(100) Writing Flash ended with an error.
File 'lpcxpresso54018_touch_cursor.axf' load failure: Ef(49): Flash driver operation gave error.
(100) Target Connection Failed
Unable to perform operation!
Command failed with exit code 1

how can I slove this problem ?

0 Kudos
Reply
1 Solution
1,763 Views
soledad
NXP Employee
NXP Employee

Hi, 

Could you please let me know which project are you using?, please try placing the MCU in ISP mode and then try launching the debug session, you can find more information on this link:

 

Regaining debug access to target MCU 


Hope it helps!

Regards

Soledad

View solution in original post

0 Kudos
Reply
2 Replies
1,764 Views
soledad
NXP Employee
NXP Employee

Hi, 

Could you please let me know which project are you using?, please try placing the MCU in ISP mode and then try launching the debug session, you can find more information on this link:

 

Regaining debug access to target MCU 


Hope it helps!

Regards

Soledad

0 Kudos
Reply
1,763 Views
seamas
Contributor I

Hi Soledad,


thanks for your help.

When I found this problem is using my test project.

I followed your suggetions to replace the MCU in ISP mode, but problem still exists.


Thanks a lot,
Seamas


0 Kudos
Reply