I can not program file into flash by MCUXpressIDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I can not program file into flash by MCUXpressIDE

跳至解决方案
1,925 次查看
seamas
Contributor I

I can not program file into flash by MCUXpressIDE, here is some log about this situation,

ProgramPage (0x10000000, 0x2208, 0x4000) status 0x1 - driver reported driver error - EXTSPI driver rc 128 (0x80)
Closing flash driver LPC540xx_SPIFI_SFDP.cfx
(100) Writing Flash ended with an error.
File 'lpcxpresso54018_touch_cursor.axf' load failure: Ef(49): Flash driver operation gave error.
(100) Target Connection Failed
Unable to perform operation!
Command failed with exit code 1

how can I slove this problem ?

0 项奖励
回复
1 解答
1,775 次查看
soledad
NXP Employee
NXP Employee

Hi, 

Could you please let me know which project are you using?, please try placing the MCU in ISP mode and then try launching the debug session, you can find more information on this link:

 

Regaining debug access to target MCU 


Hope it helps!

Regards

Soledad

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,776 次查看
soledad
NXP Employee
NXP Employee

Hi, 

Could you please let me know which project are you using?, please try placing the MCU in ISP mode and then try launching the debug session, you can find more information on this link:

 

Regaining debug access to target MCU 


Hope it helps!

Regards

Soledad

0 项奖励
回复
1,775 次查看
seamas
Contributor I

Hi Soledad,


thanks for your help.

When I found this problem is using my test project.

I followed your suggetions to replace the MCU in ISP mode, but problem still exists.


Thanks a lot,
Seamas


0 项奖励
回复