I can not program file into flash by MCUXpressIDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I can not program file into flash by MCUXpressIDE

ソリューションへジャンプ
1,863件の閲覧回数
seamas
Contributor I

I can not program file into flash by MCUXpressIDE, here is some log about this situation,

ProgramPage (0x10000000, 0x2208, 0x4000) status 0x1 - driver reported driver error - EXTSPI driver rc 128 (0x80)
Closing flash driver LPC540xx_SPIFI_SFDP.cfx
(100) Writing Flash ended with an error.
File 'lpcxpresso54018_touch_cursor.axf' load failure: Ef(49): Flash driver operation gave error.
(100) Target Connection Failed
Unable to perform operation!
Command failed with exit code 1

how can I slove this problem ?

0 件の賞賛
返信
1 解決策
1,713件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

Could you please let me know which project are you using?, please try placing the MCU in ISP mode and then try launching the debug session, you can find more information on this link:

 

Regaining debug access to target MCU 


Hope it helps!

Regards

Soledad

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,714件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

Could you please let me know which project are you using?, please try placing the MCU in ISP mode and then try launching the debug session, you can find more information on this link:

 

Regaining debug access to target MCU 


Hope it helps!

Regards

Soledad

0 件の賞賛
返信
1,713件の閲覧回数
seamas
Contributor I

Hi Soledad,


thanks for your help.

When I found this problem is using my test project.

I followed your suggetions to replace the MCU in ISP mode, but problem still exists.


Thanks a lot,
Seamas


0 件の賞賛
返信