Hi all,
when I try to use the Program/Erase flash Options direct from MCUXpresso or by using the "GUI Flash Tool" but the MCU has entered into a power low mode, the Debugger is not able to connect with the MCU.
That works without problems when I use the Debug option direct, and the GUI Flash Option works when the MCU is not in Power Low mode.
But I do not want to Debug the Code each time but use direct the Flash Option to change between several Applications.
Is it possible?
Thanks in advance