imxRT117x FlexSPI pin configuration in IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imxRT117x FlexSPI pin configuration in IDE

跳至解决方案
3,406 次查看
Jaivarthan
Contributor II

I have been trying to configure the FlexSPI pins of the iMxRT117x processor using the MCU IDE tool.

I am using the Pin cofig tool within the IDE to configure the pins. When I configured the GPIO_SD_B2_07 for FLEXSPI1_A_CLK. I expect the code to be generated with the PIN mux value of 1 as per the reference manual. But it generates as below:

IOMUXC_SetPinMux(
IOMUXC_GPIO_SD_B2_07_FLEXSPI1_A_SCLK, 0U); /* GPIO_SD_B2_07 is configured as FLEXSPI1_A_SCLK */

This looks contradicting.

0 项奖励
回复
1 解答
3,400 次查看
jaredm
Contributor III

Hi Jaivarthan,

If you browse to the definition of IOMUXC_GPIO_SD_B2_07_FLEXSPI1_A_SCLK, you will see that it is defined as 5 values. The second of these values should be a '0x1U' as indicated in the Reference Manual.

For example, in one of my RT1052 projects, this is how FlexSPI clock is defined:

    #define IOMUXC_GPIO_SD_B1_07_FLEXSPIA_SCLK 0x401F81F0U, 0x1U, 0x401F84C8U, 0x0U, 0x401F83E0U

jaredm

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,401 次查看
jaredm
Contributor III

Hi Jaivarthan,

If you browse to the definition of IOMUXC_GPIO_SD_B2_07_FLEXSPI1_A_SCLK, you will see that it is defined as 5 values. The second of these values should be a '0x1U' as indicated in the Reference Manual.

For example, in one of my RT1052 projects, this is how FlexSPI clock is defined:

    #define IOMUXC_GPIO_SD_B1_07_FLEXSPIA_SCLK 0x401F81F0U, 0x1U, 0x401F84C8U, 0x0U, 0x401F83E0U

jaredm

0 项奖励
回复
3,374 次查看
Jaivarthan
Contributor II

Hi @jaredm 

Thank you for your reply.

I see now the it is defined as below and has FlexSPI CLK pin configured in the config register by default even though I donot specifically configure it via the tool.

#define IOMUXC_GPIO_SD_B2_07_FLEXSPI1_A_SCLK 0x400E81D0U, 0x1U, 0x400E8574U, 0x1U, 0x400E8414U

 

Thanks,

Jai

0 项奖励
回复