MCUXpresso Config Tools Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Config Tools Knowledge Base

Labels

Discussions

Sort by:
  A Digital Rights Management (DRM) use case   In the Creating Secure and Non-Secure projects tutorial, you have attempted to access a Secure (S) FlexComm0 (USART) peripheral from a Non-Secure (NS) code and failed with the SecureFault exception. This was expected, as TrustZone® for ARM®v8-M protects Secure resources from Non-Secure access.   Now imagine a use case where the platform manages (protects) access to all its peripherals and firmware logic and requires all 3 rd party extensions, for example plugins or widgets, to be certified (approved) for use. The result of this approval process is some form of identification, a license key for instance, the untrusted code needs to supply to the trusted code to gain peripheral access and be able to communicate via USART. This kind of behavior can be achieved with the help of Non-Secure Callable (NSC) memory.   NSC is a type of Secure memory exclusively permitted to hold the Secure Gateway (SG) instruction that allows transition from NS to S state. When a Non-Secure program calls a function in the Secure side, the first instruction in the API must be an SG instruction. The Branch with exchange to Non-secure state (BXNS) will return execution to the Non-Secure side after the API call. While it’s possible for NSC memory to contain entire functions, its typical usage is holding tables of SG instructions with entry points, called veneers.   With GCC, ARMCC, ARMCLANG, IARCC, and LLVM compilers, you must specify the __attribute__((cmse_nonsecure_entry)) function attribute to declare an entry C/C++ function callable from NS state; SG and BXNS instructions are generated automatically. GNU linker puts the resulting code into the .gnu.sgstubs section aligned at 32 bytes.   With the solution outlined, you can reuse projects from the “TEE projects creation” tutorial to speed things up. To extend an existing project with NSC functions, the workflow is as follows: Secure state Configure project and  SAU/IDAU Implement NSC functions Generate NSC library Non-Secure state Configure project (import NSC library) Implement calls for Secure code     S project update   Start with the Secure project conveniently named “Secure”. Reserve some flash memory space for SG_veneer_table first. Navigate to Project > Properties > C/C ++ Build. Locate the MCU settings in SDK MCUs. Click Add Flash and add SG_veneer_table at 0x1000fe00, size 0x200 bytes. Click Apply.   To tell the MCU Linker to generate the NSC import library, navigate to Project > Properties > C/C ++ Build > Settings > MCU Linker > TrustZone. Select the Enable generation of Secure Gateway Import Library checkbox. Click Apply and Close.   Now setup the newly added flash memory region as NSC in the TEE tool. To switch to the TEE tool, click the Open MCUXpresso Configuration button in the Project Explorer, and select Open TEE.   The TEE tool is capable of importing project-wide memory regions from multiple projects at once. To import memory regions, click the Import button in the User Memory Regions view.   In the Select Project dialog, select both NonSecure and Secure projects and click OK.   Quick-fix the reported error Issue: SAU+IDAU: The following security requirements are not satisfied: NS_CALLABLE by right-clicking the cell and selecting the quick-fix from the context menu.   To save the changes, click Update Code.   MCUXpresso IDE v11.3.0 and earlier versions contain a bug that messes up linker script and puts SG veneers into PROGRAM_FLASH instead of SG_veneer_table when you’re modifying an existing project. To work around the problem, navigate To Project > Properties > C/C ++ Build > Settings > MCU Linker > Managed Linker Script. Deselect the Manage linker script checkbox and click Apply and Close.   Edit the script manually by opening the Debug/Secure_Debug.ld inside the IDE, find the .gnu.sgstubs section and direct it to SG_veneer_table instead of PROGRAM_FLASH.         NS project update   If you attempt to build the S project now, you’ll receive several linker errors telling you the NSC library could not be built as there are no NSC functions (yet) including the name of the said library: Secure_CMSE_lib.o. You’re going to use it to configure the Non-Secure project named “Non-Secure”. Navigate to Project > Properties > C/C ++ Build > Settings > MCU Linker > TrustZone. Click the Import button next to the Secure Gateway Import Library field, and select Workspace.   In the Input Secure Gateway Import Library dialog, select Secure_CMSE_lib.o and click OK.   You will see “${workspace_loc:/Secure/Debug/Secure_CMSE_lib.o}” in the Secure Gateway Import Library field of the MCU Linker Setting dialog.     NSC API   The source/Secure.c file already contains the sendSecureByte function implementation you need to make accessible through the NSC space. What’s missing is a few lines of code for its NSC equivalent and function prototype. Create source/nsc_api.h and source/nsc_api.c files in the Secure project workspace. The following code needs go into the newly created header file. #ifndef NSC_API_H_ #define NSC_API_H_ #include <stdint.h> void sendSecureByteNSC(uint8_t data); #endif /* NSC_API_H_ */ Add the following code into the source file. #include <arm_cmse.h> #include "fsl_debug_console.h" #include "nsc_api.h" #include "comm.h" void __attribute__((cmse_nonsecure_entry)) sendSecureByteNSC(uint8_t data) { if (cmse_nonsecure_caller()) { PRINTF("sendSecureByteNSC called from NS space\r\n"); } else { PRINTF("sendSecureByteNSC called from S space\r\n"); } sendSecureByte(data); } To rebuild the Secure project and generate the NSC import library click the Build ‘Debug’ for project ‘Secure’ button in the Toolbar.   Next in line is the Non-Secure project. The NSC library is already set to be imported. Copy Secure/source/nsc_api.h to the NonSecure/source folder. Call the sendSecureByteNSC function instead of USART_WriteByte from source/NonSecure.c. #include "nsc_api.h" …                   USART_WriteByte((USART_Type *)FLEXCOMM0, 'n'); sendSecureByteNSC('n'); Rebuild the Non-Secure project and debug both. Select the Secure project in the workspace and select Debug either from the Quickstart panel or the project context menu. Once the code is running, each press of the WAKEUP (S2) button on the LPCXpresso55S69 board will display the “sendSecureByteNSC called from NS space” message in the IDE console and send a single character via USART instead of failing with the SecureFault exception.    
View full article
Creating Secure and Non-Secure projects The LPC55S69 MCU series contains Arm TrustZone® and Trusted Execution Environment extension from NXP. It allows users to assign cores, memories, and peripherals to the Secure or the Non-Secure World and restrict access between them. Manufacturers can use it to secure critical functionality of a device. For example, the Secure code is provided on the device by the manufacturer and could not be modified by users. However, a user can create a Non-Secure application and download it to the device. A secure code can communicate over a channel which security cannot be exposed to the Non-Secure World. This example is shown in the tutorial. This tutorial demonstrates how to create Secure and Non-Secure projects and their basic configuration using MCUXpresso IDE and Config Tools. LPCXpresso55S69 Board is used for the demonstration of functionality. Project description Two projects, a Secure and a Non-Secure, are created. Both projects are used on a single core. USART is used for sending data and it is configured as a Secure peripheral. S1 (ISP) button is used for sending data from the Secure world. S2 (WAKEUP) button is used for sending data from the Non-Secure world, which is not allowed due to a security violation. Prerequisites MCUXpresso IDE 11.3.0 LPCXpresso55S69 SDK 2.9.0 LPCXpresso55S69 Board You are familiar with the security extension used on LPC55S69. You are familiar with MCUXpresso IDE and Config Tools – Getting started with TEE. Steps 1.  Create a Secure project Create a new project, select the security type (Secure), and set memory regions in New Project Wizard. You must do it as Secure and Non-Secure projects use different parts of memories. In addition, secure memories use aliases – the 28 th bit is set to 1.  To download the firmware to the secure flash, select the Secure flash driver „LPC55xx_S.cfx“. 2. Create a Non-Secure project Create a new project and set security and memories as follows. 3. Connect the projects It is not mandatory but it makes things easier. Reference the Secure project from the Non-Secure project. It makes importing memory regions into the TEE tool easier.  The current and the linked or linking projects are preselected in the import dialog. In the  Secure project set the Non-Secure project to be preprogrammed.  Both projects are automatically downloaded to the board prior to debugging the Secure project. 4. Disable generation of  a Secure gateway library This feature is not used in this tutorial, therefore it must be turned off to compile the project. Change it in project properties (right-click the project and select Properties). 5. Route Secure pins Open Pins tool. Route S1 pin to SECGPIO. For detecting button press, peripheral SPINT is used and it must be routed to the same pin. Flexcom, which is used as USART, is routed by default in a board configuration. Do not change anything there. 6. Setup Secure peripherals Flexcomm is used for USART communication. Open Peripherals tool. Add USART component in Peripherals tool. Use the default configuration. Problems related to clocks must be resolved in the Clocks tool by enabling peripheral clock. Right-click the problem in Problems view and select Show problem. It opens the Clocks tool and highlights the problematic clock path. Add PINT component. Uncheck the checkbox „Show only components in toolchain project“  as the PINT driver is not in the project yet. Otherwise, it is not listed in the dialog. Select SECPINT peripheral. Configure it to invoke a callback function upon falling edge is detected on S1. Add the  PINT driver to the project via quick-fix in the Problems view. 7. Setup security extension in TEE tool Import memory regions from both projects in the User Memory Regions tab. As nothing is configured for the security extension, there are errors and warnings in the Security Level column. In Security Access Configuration, Miscellaneous tab enable Secure check for AHB matrix and Non-Secure access to floating point extension (CP10 access). FPU is turned on by default. Enable SAU and set Non-Secure regions. Other memory is considered Secure. Set MPC to allow only Secure transactions for Secure memory regions. It resolves errors and warnings in User Memory regions. Set SECGPIO and SECPINT peripherals as Secure. Keep Flexcomm as Non-Secure for now for demonstration purposes. Set PINT interrupt security as Non-Secure. Sending data from the Non-Secure world is also triggered by button press so its interrupt security must be set accordingly. It is the last setting of the Secure project in Config Tools, at this stage update the code. 8. Update Secure project settings After updating the code, create a  TrustZone folder. By default, new folders are excluded from the build. Right-click the folder and uncheck Exclude resource from build in the folder properties. Add the path to the folder into Include paths in project settings. 9. Add missing drivers If you use this version of tools,  add the inputmux driver in the Secure project. It is required for code generated by the Pins tool. 10. Update the Secure source code Do the following updates in source/Secure.c file. Add TEE initialization function call. As security is the first thing that should be configured,  place it SystemInitHook function. This way it is called before entering the main function. The initialization function is implemented in resource_config.h which must be included.       /*! * @brief Application-specific implementation of the SystemInitHook() * weak function. */ void SystemInitHook(void) { BOARD_InitTEE(); }       Implement SECPINT callback function. After pressing S1,  some data is sent from the Secure world via USART. For simplicity, character ‚s‘ is sent from the Secure world and character ‚n‘  is sent from the Non-Secure world.       /* * @brief Send on byte over secure channel * @param data data to be sent */ void sendSecureByte(uint8_t data) { USART_WriteByte(FLEXCOMM0_PERIPHERAL, data); } /* * @brief S1 button interrupt callback * @param pintr pin interrupt type * @param pmatch_status match status */ void secureButtonCallback(pint_pin_int_t pintr ,uint32_t pmatch_status) { sendSecureByte('s'); }       When you do the initialization in the Secure world, the MCU can continue with executing instructions from the Non-Secure world. The switching consists of setting a Non-Secure stack, a vector table, and calling a reset handler. The Non-Secure flash was previously configured to start at address 0x10000.       /* Start address of Non-secure application */ #define NON_SECURE_START 0x10000 /* typedef for non-secure callback functions */ typedef void (*funcptr_ns)(void) __attribute__((cmse_nonsecure_call)); int main(void) { /* Init board hardware. */ BOARD_InitBootPins(); BOARD_InitBootClocks(); BOARD_InitBootPeripherals(); #ifndef BOARD_INIT_DEBUG_CONSOLE_PERIPHERAL /* Init FSL debug console. */ BOARD_InitDebugConsole(); #endif PRINTF("Secure World\n"); /* Set non-secure main stack (MSP_NS) */ __TZ_set_MSP_NS(*((uint32_t *)(NON_SECURE_START))); /* Set non-secure vector table */ SCB_NS->VTOR = NON_SECURE_START; /* Get non-secure reset handler */ funcptr_ns ResetHandler_ns; ResetHandler_ns = (funcptr_ns)(*((uint32_t *)((NON_SECURE_START) + 4U))); /* Jump to normal world */ ResetHandler_ns(); /* Force the counter to be placed into memory. */ volatile static int i = 0 ; /* Enter an infinite loop, just incrementing a counter. */ while(1) { i++ ; /* 'Dummy' NOP to allow source level single stepping of tight while() loop */ __asm volatile ("nop"); } return 0 ; }       11. Route Non-Secure pins Configure the Non-Secure project properly. Route S2 pin to GPIO as input. Route  PINT for pin #64. Flexcomm is routed by default, remove this routing as it is already routed in the Secure project. 12. Setup Non-Secure peripherals Set up PINT to use callback on falling edge of the S2 button press.  Add the driver, for example, via quick fix. 13. Update the Non-Secure source code Keep the initialization of Pins and Peripherals and remove the other initialization as it was done in the Secure world. That also includes the overriding SystemInit function.       /* * @brief System initialization * * Intentionally empty. Required initialization was done in the Secure project. * */ void SystemInit(void) { } /* * @brief Application entry point. */ int main(void) { /* Init board hardware. */ BOARD_InitBootPins(); BOARD_InitBootPeripherals(); ...       Add the code for sending data from the Non-Secure world. To use the USART_WriteByte function and the imputmux driver, include fsl_usart.h.       /* * @brief S2 button interrupt callback * @param pintr pin interrupt type * @param pmatch_status match status */ void nonSecureButtonCallback(pint_pin_int_t pintr ,uint32_t pmatch_status) { USART_WriteByte((USART_Type *)FLEXCOMM0, 'n'); }       Now the projects are ready. When debug is executed for the Secure project, the Non-Secure project is also downloaded to the board. After pressing S1, 's' is sent from the Secure world. When S2 is pressed, 'n' is sent from the Non-Secure world because Flexcomm is configured as Non-Secure in the TEE tool. 14. Securing USART Open the TEE tool from the Secure project and set the Flexcomm slave as Secure. After this change, you can send data from the Secure world but an attempt to send data from the Non-Secure world results in bus fault.  
View full article
This tutorial is how to start working with TEE
View full article
The MCUXpresso Config Tools is an integrated suite of configuration tools that help guide users from first evaluation to production software development when designing with Arm ® Cortex ® -M-based devices from NXP, including its general purpose, crossover and wireless-enabled MCUs. These configuration tools allow developers to quickly build a custom SDK and leverage pins, clocks and peripherals to generate initialization C code for custom board support. The following tutorials help you design with the MCUXpresso software and tools. Pins Tool and Expansion Headers Apply Arduino virtual adapter into compatible header Measuring temperature using digital sensor DS18B20 and Arduino Multifunction Shield on FRDM K64F Creating expansion board definition file for Arduino Multifunction shield Adding Expansion Headers to a custom board Peripherals tool USB Audio Class Tutorial  Using TDA1543 I2S DAC with the LPC54114 board  Touch controlled led light on LPCXPRESSO845-BRK  eDMA component abilities shown on ADC measurement example Trusted Execution Environment (TEE) Getting started with TEE  Creating Secure and Non-Secure projects Calling Secure code from Non-Secure region LPC55Sxx: Securing Digital IO Pins
View full article
The following article has quick steps and videos how to get started with Kinetis Expert SDK and Design Studio:   https://community.freescale.com/docs/DOC-329662   Enjoy!
View full article
The following article describes how to configure code generation for the clock gates and how to perform a full initialization with the Pins Tool: https://mcuoneclipse.com/2016/07/19/nxp-pins-tool-clock-gates-and-controlling-the-bits/  
View full article