can´t connect with KinetisFlashTool to mkl17z32vlh4 ROM Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can´t connect with KinetisFlashTool to mkl17z32vlh4 ROM Boot

Jump to solution
5,781 Views
marianoT
Contributor III

hi, using KinetisFlashTool can´t connect with mkl17z32vlh4 ROM boot, using UART. I get the same behaviour with a custom host.

this is the log of KinetisFlashTool:

[5a a6]
<5a>
Ping responded in 1 attempt(s)
<a7>
<00 01 01 50 00 00 78 04>
Framing protocol version = 0x50010100, options = 0x0
inject command 'get-property'
[5a a4 0c 00 6c 3c 07 00 00 02 05 00 00 00 ee cc a2 77]
<>
<>
<>
<>
<>
Error: read_start_byte() timeout after 5.107 seconds
sendCommandGetResponse.writePacket error 5.
processResponse: null packet
- took 5.109 seconds
[5a a6]
<e0>
<5f>
<04>
<10>
<03>
<01>
<e7>
<00>
<00>
<e4>
<>
[5a a6]
<5a>
Ping responded in 1 attempt(s)
<a7>
<00 01 01 50 00 00 78 04>
Framing protocol version = 0x50010100, options = 0x0
inject command 'get-property'
[5a a4 0c 00 6c 3c 07 00 00 02 05 00 00 00 ee cc a2 77]
<>
<>
<>
<>
<>
Error: read_start_byte() timeout after 5.107 seconds
sendCommandGetResponse.writePacket error 5.
processResponse: null packet
- took 5.109 seconds
[5a a6]
<5a>
Ping responded in 1 attempt(s)
<a7>
<00 01 01 50 00 00 78 04>
Framing protocol version = 0x50010100, options = 0x0
inject command 'get-property'
[5a a4 0c 00 6c 3c 07 00 00 02 05 00 00 00 ee cc a2 77]
<>
<>
<>
<>
<>
Error: read_start_byte() timeout after 5.106 seconds
sendCommandGetResponse.writePacket error 5.
processResponse: null packet
- took 5.107 seconds
[5a a6]
<5a>
Ping responded in 1 attempt(s)
<a7>
<00 01 01 50 00 00 78 04>
Framing protocol version = 0x50010100, options = 0x0
inject command 'get-property'
[5a a4 0c 00 6c 3c 07 00 00 02 05 00 00 00 ee cc a2 77]
<>
<>
<>
<>
<>
Error: read_start_byte() timeout after 5.106 seconds
sendCommandGetResponse.writePacket error 5.
processResponse: null packet
- took 5.107 seconds

0 Kudos
Reply
1 Solution
5,697 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

1. Please try the get property command on KL17Z by using  blhost, to check the flash sector size and flash size. Refer to the blhost User's Guide, chaperter 4.2.2.

Here is the log for KL27Z:

blhost.jpg

 

2.For internal flash memory, memory ID should be 0, not 0x01. 

3. blhost download:  https://www.nxp.com/mcuboot

View solution in original post

0 Kudos
Reply
7 Replies
5,649 Views
marianoT
Contributor III

Hi Robin, it works connecting directly to the PC, the communication with host uC and  mkl17z32vlh4 works fine, i think maybe the signal is noisy, so ROM boot protocol fail.

thanks for your time and sorry.

best regards. 

Mariano

0 Kudos
Reply
5,771 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi marianoT,

Please check if PTA1 and PTA2 are connect. These two pins are the default UART pads used by the Kinetis ROM Bootloader.

Table 13-1. Kinetis Bootloader Peripheral Pinmux.jpg
Press PTA4(NMI_b) pin before power on, then click the Connect button on KinetisFlashTool.

13.3.3 Start-up Process.jpg

I don't have mkl17z32vlh4 by my side, so I tested it on the FRDM-KL27Z development board.
1. Press SW1
2. Plug the USB cable to J13

FRDM-KL27Z KinetisFlashTool.jpg

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply
5,766 Views
marianoT
Contributor III

hi, Robin_shen, if you look in the log i posted, the ping cmd execute succesfully always,

 [5a a6]
<5a>
Ping responded in 1 attempt(s)
<a7>
<00 01 01 50 00 00 78 04>

then command 'get-property' fail to execute
[5a a4 0c 00 6c 3c 07 00 00 02 05 00 00 00 ee cc a2 77]

 

thanks

0 Kudos
Reply
5,754 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry for my last reply!
According to the "Table 5-2. GetProperty Command Packet Format (Example)", Memory ID should be 0x01 for internal flash. But I don't know why it send 0x77a2ccee.

Table 5-2. GetProperty Command Packet Format (Example).jpg

By compare the log of FRDM-KL27Z(0x03fffad8), this is the only difference.

compare log.jpg


The FRDM-KL27Z is able to successful response to command 'get-property(flash-sector-size)'
But your KL17 did not send back ACK.

Table 14-1. Tag values GetProperty and SetProperty.jpg

0 Kudos
Reply
5,732 Views
marianoT
Contributor III

hi, Robin, i send the commands using serial port and it doesn´t respond: 


16:39:48.243 [TX] - 5A A6  -> Ping CMD
16:39:48.784 [RX] - 5A A7 00 01 01 50 00 00 78 04 -> Ping Response
16:39:49.884 [TX] - 5A A4 0C 00 E9 06 07 00 00 02 05 00 00 00 D8 FA FF 03 -> get Property
16:39:51.099 [TX] - 5A A4 0C 00 E9 06 07 00 00 02 05 00 00 00 D8 FA FF 03 -> get Property

0 Kudos
Reply
5,698 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

1. Please try the get property command on KL17Z by using  blhost, to check the flash sector size and flash size. Refer to the blhost User's Guide, chaperter 4.2.2.

Here is the log for KL27Z:

blhost.jpg

 

2.For internal flash memory, memory ID should be 0, not 0x01. 

3. blhost download:  https://www.nxp.com/mcuboot

0 Kudos
Reply
5,691 Views
marianoT
Contributor III

Hi Robin, thanks, i try but it doesn´t work,

i test it at different baud rates (115200,19200,9600), also put a pull up resistor on LPUART RX, but i only get PING response.

LOG:

PS D:\MCUXpressoIDE_10.2.0_759\workspace\blhost_2.6.6\bin\win> .\blhost.exe -p com2,115200 -d -- get-property 5
[5a a6]
<5a>
Ping responded in 1 attempt(s)
<a7>
<00 01 01 50 00 00 78 04>
Framing protocol version = 0x50010100, options = 0x0
Inject command 'get-property'
[5a a4 0c 00 26 3c 07 00 00 02 05 00 00 00 00 00 00 00]
<>
<>
<>
<>
<>
Error: read_start_byte() timeout after 5.110 seconds
sendCommandGetResponse.writePacket error 5.
processResponse: null packet
- took 5.113 seconds
Response status = 10004 (0x2714) No response packet from target device.
PS D:\MCUXpressoIDE_10.2.0_759\workspace\blhost_2.6.6\bin\win> .\blhost.exe -p com2,115200 -d -- get-property 4
[5a a6]
<5a>
Ping responded in 1 attempt(s)
<a7>
<00 01 01 50 00 00 78 04>
Framing protocol version = 0x50010100, options = 0x0
Inject command 'get-property'
[5a a4 0c 00 f5 7b 07 00 00 02 04 00 00 00 00 00 00 00]
<>
<>
<>
<>
<>
Error: read_start_byte() timeout after 5.106 seconds
sendCommandGetResponse.writePacket error 5.
processResponse: null packet
- took 5.112 seconds
Response status = 10004 (0x2714) No response packet from target device.

0 Kudos
Reply