Bootloader SDK for S32K148EVB-Q176

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Bootloader SDK for S32K148EVB-Q176

跳至解决方案
2,899 次查看
Chandra13
Contributor I

Hello,

  1. Is there a bootloader SDK available for the S32K148? I tried Select Board | MCUXpresso SDK Builder (nxp.com), but I could not find the specific configuration.
  2. For now, I use the Design Studio 3.4 to work on other topics (SPI, CAN, LIN). Do I need to download the MCUXpresso IDE to work on the bootloader topics?
0 项奖励
回复
1 解答
2,890 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Chandra13

1. We do not provide such SDK to customers, only some application notes and demos, these demos are based on the old version of the SDK, and cannot be directly run on the new version of the IDE, such as S32 V3.4.

AN12218: S32K1xx Bootloader – Application Note  

AN12323: S32K1xx Firmware updates – Application Note  

Unified bootloader Demo 


2. MCUXpresso IDE has nothing to do with S32K.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,891 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Chandra13

1. We do not provide such SDK to customers, only some application notes and demos, these demos are based on the old version of the SDK, and cannot be directly run on the new version of the IDE, such as S32 V3.4.

AN12218: S32K1xx Bootloader – Application Note  

AN12323: S32K1xx Firmware updates – Application Note  

Unified bootloader Demo 


2. MCUXpresso IDE has nothing to do with S32K.

0 项奖励
回复
1,759 次查看
CHYYDS
Contributor II

@Senlent Hello, do you have any information or documents related to bootloader for S32K344? Can you provide a link? Thank you very much!

0 项奖励
回复