Hi,
I've several question about the use of the MCUBOOT via CANBUS listed below.
1) I looked that there is a particular application called BusPal that works as a bridge. It run in an intermediate MCU and
traduce UART packet from the blhost on PC to target MCU. The BusPal project is located on NXP_Kinetis_Bootloader_2_0_0. Is it still compatible with the new version of MCUBoot located on MCUXpressoSDK like 2.7.0 version?
2) Is BusPal easily ported to other MCU?
3) Is there a manner to try MCUBoot can porting directly with PC (without BusPal bridge)?
What I had thought was to use a cpu arm with linux OS which already integrates a can controller like IMX8.
However, Blhost is already compiled only for x86 systems. Is it possible to compile it also for ARM and to use the solution I have in mind or are there problems?
Thank you in advance!